+15,00,000 products in offer
7,000 packages per day
+3,00,000 clients from 150 countries
Radio engineering is a field of technology and science dealing with the generation, transmission, reception and processing of electromagnetic waves, mainly in the radio frequency range. It covers a wide range of issues related to the transmission of information at a distance without the use of a physical wire connection, using the phenomena of propagation of radio waves in the atmosphere, space or other media.
The basis of radio engineering is the use of physical phenomena that enable the emission and reception of electromagnetic waves, such as electromagnetic induction, resonance, modulation and demodulation of signals, attenuation, diffraction and reflection. The key components of radio engineering systems are transmitters, receivers, Antennas, amplifiers, frequency generators and filtering and mixing systems. Radio engineering is based on the precise selection of transmission parameters, such as carrier frequency, bandwidth, transmit power or modulation type.
In practice, radio technology is used in telecommunications, broadcasting, television, radio navigation, radiolocation, military communication systems, data transmission and wireless technologies such as Wi-Fi, Bluetooth or satellite systems. Its development has enabled the emergence of modern mobile networks, GPS systems, radar and Internet of Things.
Modern radio technology combines traditional analogue circuits with modern digital systems, enabling the implementation of complex modulation algorithms, data compression, correction coding and adaptive adjustment of transmission parameters. Advances in microwave technology, signal processing and the miniaturisation of electronic components are significantly expanding the design and operational possibilities of radio systems, making radio engineering a key branch of modern communications engineering.
Transfer Multisort Elektronik (TME) is one of the world’s largest global distributors of electronic components, electrotechnical parts, workshop equipment, and industrial automation. The catalog includes over 1,500,000 products from 1,300 leading manufacturers. TME’s modern logistics centers in Łódź and Rzgów (Poland), with a combined area of over 40,000 m², ship nearly 6,000 packages daily to customers in more than 150 countries.
TME also invests in the development of knowledge and skills of young engineers and electronics enthusiasts through the TME Education project, and supports the tech community by organizing the TechMasterEvent series, promoting innovation and experience exchange.