+15,00,000 products in offer
7,000 packages per day
+3,00,000 clients from 150 countries
A commutator motor is a type of electric motor in which the change of current direction in the rotor windings is realised by means of a mechanical commutator - an annular assembly of brushes and copper segments. This design makes it possible to operate both on direct current (DC) , and - in the case of some versions - alternating current (AC), making commutator motors versatile in variable load applications.
In the classic commutator motor system, the rotor has windings through which current flows, supplied by brushes pressed against a rotating commutator. The interaction of the magnetic field of the stator with the currents in the rotor windings results in an electrodynamic force that generates torque. The role of the commutator is to cycle the winding circuits so that the torque remains in line with the direction of rotation, regardless of the position of the rotor.
The advantage of commutator motors is their ability to achieve high starting torque and the ease of speed control by varying the supply voltage. Due to these properties, they are often used in portable appliances, power tools, household appliances and applications with high dynamic requirements. The universal (AC/DC) versions allow operation with alternating voltage, which simplifies the design of household appliances and power tools.
However, mechanical commutation is also associated with certain limitations - notably brush wear and sparking on the commutator, which affects durability and can generate electromagnetic interference. For this reason, they are increasingly being replaced in modern systems by brushless electronically commutated Actuators. Nevertheless, commutator motors remain popular in many applications due to their simplicity, low production costs and wide range of applications.
Transfer Multisort Elektronik (TME) is one of the world’s largest global distributors of electronic components, electrotechnical parts, workshop equipment, and industrial automation. The catalog includes over 1,500,000 products from 1,300 leading manufacturers. TME’s modern logistics centers in Łódź and Rzgów (Poland), with a combined area of over 40,000 m², ship nearly 6,000 packages daily to customers in more than 150 countries.
TME also invests in the development of knowledge and skills of young engineers and electronics enthusiasts through the TME Education project, and supports the tech community by organizing the TechMasterEvent series, promoting innovation and experience exchange.