+15,00,000 products in offer

7,000 packages per day

+3,00,000 clients from 150 countries

Quick Buy Favourites
Cart

Soft start - definition

Soft start is a technique for controlling the start-up of electrical equipment by gradually increasing the supply voltage or current to allow a softer start-up of the load, usually an electric motor. The aim of this method is to reduce the current and mechanical surges that occur when the full voltage supply is directly switched on, which can lead to overloads, excessive wear on components or interference with the power grid.

In practice, soft start is implemented using specialised electronics, such as Thyristors or power transistors, which modulate the output voltage in a controlled manner. The parameters of the start-up process - duration, voltage ramp-up speed or starting torque limit - are adapted to the characteristics of the device and the application requirements. The operation of the system can also include control of coasting or soft stop, increasing its usefulness in applications requiring precise and safe energy management.

Soft start is mainly used in Actuators induction motors, pumps, fans, compressors and wherever dynamic loads can affect the durability of the mechanics or the stability of the mains supply. Compared to direct start systems or those using starting transformers, soft start technology offers greater flexibility and improved performance, without the need for mechanical components. In modern installations, it is often integrated into Automation systems, enabling remote management and diagnostics of the start-up process.

Transfer Multisort Elektronik (TME) is one of the world’s largest global distributors of electronic components, electrotechnical parts, workshop equipment, and industrial automation. The catalog includes over 1,500,000 products from 1,300 leading manufacturers. TME’s modern logistics centers in Łódź and Rzgów (Poland), with a combined area of over 40,000 m², ship nearly 6,000 packages daily to customers in more than 150 countries.

TME also invests in the development of knowledge and skills of young engineers and electronics enthusiasts through the TME Education project, and supports the tech community by organizing the TechMasterEvent series, promoting innovation and experience exchange.

READ ALSO