+15,00,000 products in offer

7,000 packages per day

+3,00,000 clients from 150 countries

Quick Buy Favourites
Cart

Ballasts - definition

Ballast is an electrical or electronic device used in power supply systems for discharge light sources, such as fluorescent, sodium, mercury vapour or metal halide lamps, to regulate and stabilise the electrical current flowing through the lamp during operation. In discharge lamps, at the moment of ignition, there is a very low resistance, which, without proper control, could lead to an excessive increase in current and, consequently, damage to the Light sources. Ballasts limit the current to a safe, nominal value, ensuring correct lamp operating conditions and lamp life.

In classical solutions, the ballast was in the form of an electromagnetic choke, which limited the current through its inductive properties. Modern electronic ballasts, based on semiconductor circuits, operate at high frequency, which significantly improves energy efficiency, reduces light flicker and increases comfort. Ballasts also enable functions such as smooth start, light intensity control and communication with lighting management systems.

In addition to its use in lighting technology, the term ballast is also found in the context of mechanical and aerospace systems, where it denotes an element that stabilises the movement or position of objects. In the electrical context, however, the ballast's main task remains to protect the lamp and ensure optimal operating conditions throughout its life cycle. Today's energy efficiency standards promote the use of high-efficiency ballasts, resulting in reduced energy consumption and greenhouse gas emissions.

Transfer Multisort Elektronik (TME) is one of the world’s largest global distributors of electronic components, electrotechnical parts, workshop equipment, and industrial automation. The catalog includes over 1,500,000 products from 1,300 leading manufacturers. TME’s modern logistics centers in Łódź and Rzgów (Poland), with a combined area of over 40,000 m², ship nearly 6,000 packages daily to customers in more than 150 countries.

TME also invests in the development of knowledge and skills of young engineers and electronics enthusiasts through the TME Education project, and supports the tech community by organizing the TechMasterEvent series, promoting innovation and experience exchange.

READ ALSO