+15,00,000 products in offer
7,000 packages per day
+3,00,000 clients from 150 countries
Earthing is the connection of the element of the electrical installation with the earth (ground) to provide a common reference potential and protection against the effects of surges, short circuits and lightning. It is an essential part of the electric shock protection system, allowing leakage, surge or fault currents to be safely discharged into the ground, minimising the risk of electric shock and damage to equipment.
Technically, earthing is realised through a protective conductor connecting the protected element to the earth - a metallic conductor buried in the ground or buried in foundation concrete, capable of conducting current to the ground. The impedance value of this connection is critical to the effectiveness of the protection system, including the proper tripping of RCD Circuit Breakers and the rapid dissipation of charge. Effective earthing also has the effect of reducing potential differences between points in the installation, which increases the safety of people and equipment.
Others distinguish between different types of earthing, including protective, operational, functional or lightning protection, depending on the function performed. Protective earthing mainly refers to the metal enclosures of electrical equipment and ensures that, in the event of a voltage breakthrough to their surface, the current is safely directed to earth. Operational earthing relates to the operating points of a system, e.g. the centre of a transformer, while functional earthing relates to ensuring the proper operation of electronic systems, especially for low amplitude or noise-sensitive signals.
The technical parameters of earthing are regulated by national and international standards, which define, among other things, the permissible values of earthing resistance, methods of measurement and requirements for protective systems in buildings and industrial installations. The proper implementation and periodic inspection of earthing is crucial to ensure continuity of protection and the safe operation of electrical power systems.
Transfer Multisort Elektronik (TME) is one of the world’s largest global distributors of electronic components, electrotechnical parts, workshop equipment, and industrial automation. The catalog includes over 1,500,000 products from 1,300 leading manufacturers. TME’s modern logistics centers in Łódź and Rzgów (Poland), with a combined area of over 40,000 m², ship nearly 6,000 packages daily to customers in more than 150 countries.
TME also invests in the development of knowledge and skills of young engineers and electronics enthusiasts through the TME Education project, and supports the tech community by organizing the TechMasterEvent series, promoting innovation and experience exchange.