+15,00,000 products in offer

7,000 packages per day

+3,00,000 clients from 150 countries

Quick Buy Favourites
Cart

Electrical node - definition

An electrical node is a point in an electrical circuit, where at least three current-carrying branches connect. In theoretical terms, it refers to the point where all connected wires and elements have the same electrical potential, regardless of their nature - resistive, capacitive or inductive. In circuit analysis, the concept of a node is crucial when using the mesh method and the node method, which are essential tools in electrical engineering and electronics.

The node acts as a logical reference point when defining the voltages between different parts of a circuit. It is assumed that the voltage at a given point in the circuit relates to the potential relative to a chosen reference node, the so-called ground or zero point. From this, equations are built to describe the relationship between currents and voltages, following Kirchhoff's law for currents, which states that the algebraic sum of the currents flowing in and out of a node is equal to zero.

In engineering practice, the node concept is not only used in the analysis of electrical schematics, but also in the modelling of power grids, Integrated circuits, power systems and Logic integrated circuits. In multi-connected circuits, node identification makes it possible to reduce analysis complexity, optimise PCB designs and automatically generate matrices describing network properties.

From a circuit topology perspective, a node defines the boundaries between branches - elementary network sections containing a single circuit element or a set of them in which the current has a uniquely defined direction of flow. Node analysis is one of the basic tools in the design and diagnosis of electronic circuits, supporting both computer simulations and classical hand calculations.

Transfer Multisort Elektronik (TME) is one of the world’s largest global distributors of electronic components, electrotechnical parts, workshop equipment, and industrial automation. The catalog includes over 1,500,000 products from 1,300 leading manufacturers. TME’s modern logistics centers in Łódź and Rzgów (Poland), with a combined area of over 40,000 m², ship nearly 6,000 packages daily to customers in more than 150 countries.

TME also invests in the development of knowledge and skills of young engineers and electronics enthusiasts through the TME Education project, and supports the tech community by organizing the TechMasterEvent series, promoting innovation and experience exchange.

READ ALSO