+15,00,000 products in offer
7,000 packages per day
+3,00,000 clients from 150 countries
Voltmeters is a measuring instrument used to directly measure the difference of electrical potential, or voltage, between two points in an electrical circuit. The unit measured by a voltmeter is volts (V), and the device can be used in both direct current (DC) and alternating current (AC) circuits. The voltmeter allows the evaluation of the operation of power sources, circuit components and the voltage characteristics of electronic components and electrical components.
The main feature of a voltmeter is its high input resistance, which minimises the effect of the measurement on the system under test. As a result, the current flow through the instrument is negligible, allowing the measurement to be considered non-invasive. Voltmeters are connected in parallel to the component under test, allowing a true potential difference to be obtained without interfering with the circuit.
Voltmeters come in analogue and digital versions. Analogue versions are based on a magneto-electric mechanism (e.g. with a movable angle), where the pointer swing is proportional to the voltage. Digital voltmeters use analogue-to-digital converters (ADCs), which convert the input voltage into a numerical value presented on a display. Modern Digital Multimeters act as universal voltmeters, offering additional measurement modes, automatic range selection and data logging functions.
The accuracy of voltage measurement depends on the class of instrument, its measuring range, the frequency of the signal under test and the influence of external factors such as temperature or electromagnetic interference. Specialised applications use differential, selective, high-voltage or laboratory voltmeters with improved precision and stability. Voltmeter measurement is an essential tool in the diagnosis, design and maintenance of electrical, electronic and Automation systems.
Transfer Multisort Elektronik (TME) is one of the world’s largest global distributors of electronic components, electrotechnical parts, workshop equipment, and industrial automation. The catalog includes over 1,500,000 products from 1,300 leading manufacturers. TME’s modern logistics centers in Łódź and Rzgów (Poland), with a combined area of over 40,000 m², ship nearly 6,000 packages daily to customers in more than 150 countries.
TME also invests in the development of knowledge and skills of young engineers and electronics enthusiasts through the TME Education project, and supports the tech community by organizing the TechMasterEvent series, promoting innovation and experience exchange.