+15,00,000 products in offer
7,000 packages per day
+3,00,000 clients from 150 countries
Phantom power supply is a method of supplying direct voltage to active electroacoustic components, most frequently condenser microphones and active di-boxes, through signal cables in a symmetrical standard. This mechanism eliminates the need for separate power sources, while ensuring compatibility with audio devices equipped with standard XLR or TRS inputs.
The principle of Phantom power supply is based on simultaneous transmission of power and audio signal through the same cables, this is possible thanks to the use of symmetrical signal transmission, in which the voltage is applied simultaneously on both signal cables relative to a common ground potential reference. The typical voltage used in this standard is +48V DC, although in some cases 24V or 12V variants can be found, depending on the requirements of the device being powered.
The use of appropriate limiting resistors in the circuit the use of appropriate limiting resistors in the power supply circuit ensures separation of the audio signal from the DC voltage, minimising interference and the influence of the power supply on sound characteristics. High-quality Phantom circuits are designed with respect to the impedance parameters and noise filtering, to eliminate noise and interference from poor quality Cables or unstable voltage sources.
Phantom power is implemented in professional mixers, audio interfaces and microphone preamplifiers, and its use enables condenser microphones to work properly, where the active input stage requires an external voltage for diaphragm polarisation and signal amplification. In standard configurations, it ensures compatibility with dynamic equipment, as the pickup circuit does not draw supply voltage, which allows a universal use of common input channels for Others types of microphones.
In stage and studio constructions, it is necessary to use high-quality cabling and appropriate protection against accidental application of voltage to devices not adapted to Phantom operation, as inappropriate connections can lead to damage to sensitive output circuit components, especially in the case of older or asymmetrical electronic designs. Protection systems used in modern audio circuits use Protection diodes and suppression filters, to eliminate the possibility of impulse damage to components due to uncontrolled connection or disconnection of live cables.
Car Antennas with Phantom power supply
Transfer Multisort Elektronik (TME) is one of the world’s largest global distributors of electronic components, electrotechnical parts, workshop equipment, and industrial automation. The catalog includes over 1,500,000 products from 1,300 leading manufacturers. TME’s modern logistics centers in Łódź and Rzgów (Poland), with a combined area of over 40,000 m², ship nearly 6,000 packages daily to customers in more than 150 countries.
TME also invests in the development of knowledge and skills of young engineers and electronics enthusiasts through the TME Education project, and supports the tech community by organizing the TechMasterEvent series, promoting innovation and experience exchange.