+1 500 000 products in offer

6000 packages per day

+300 000 clients from 150 countries

Quick Buy Favourites
Cart

Capacitive diodes (varactor) - definition

A Capacitive Diode (varactor) is a specialised semiconductor element whose main function is to vary capacitance depending on the voltage applied in the forward direction. Unlike standard Diodes, it is not used as a rectifier, but as a non-linear voltage-controlled capacitor. Its operation is based on changing the width of the depleted layer of the p-n junction, which acts as the dielectric of the capacitor.

As the breakdown voltage increases, the thickness of the depleted region increases, leading to a decrease in the capacitance of the junction. This phenomenon is used in electronic circuits for precise frequency control, modulation and tuning of resonant circuits. The capacitive characteristics of the varactor are non-linear, which allows dynamic tuning of the parameters of filters, generators and phase shifters in real time.

Varactors are widely used in high-frequency technology, especially in RF and microwave circuits, where their small size and high speed of response to voltage changes allow applications in modern communication systems. A suitably designed semiconductor structure and doping process influence the range of adjustable capacitance, loss and parameter stability as a function of temperature.

Due to its operation in the inverting state, the capacitive diode is characterised by a very low leakage current and high input impedance, which makes it useful in high Q systems. Typical materials used in the manufacture of varactors are silicon and gallium arsenide, which enable a wide operating bandwidth and low dielectric losses.

Capacitive Diodes

Transfer Multisort Elektronik (TME) is one of the world’s largest global distributors of electronic components, electrotechnical parts, workshop equipment, and industrial automation. The catalog includes over 1,500,000 products from 1,300 leading manufacturers. TME’s modern logistics centers in Łódź and Rzgów (Poland), with a combined area of over 40,000 m², ship nearly 6,000 packages daily to customers in more than 150 countries.

TME also invests in the development of knowledge and skills of young engineers and electronics enthusiasts through the TME Education project, and supports the tech community by organizing the TechMasterEvent series, promoting innovation and experience exchange.

READ ALSO