+1 500 000 products in offer

7000 packages per day

+300 000 clients from 150 countries

Quick Buy Favourites
Cart

Inrush current - definition

Start-up current is the instantaneous, significantly increased electrical current that flows through an electrical or electronic device when it is switched on. This phenomenon results from a sudden change in the operating conditions of the system, such as the need to overcome mechanical inertia in motors, the charging of capacitive elements in power supplies or the saturation of magnetic cores in transformers. The value of the inrush current can exceed the rated current by several times, and its duration depends on the characteristics of the load and the parameters of the power source.

In AC Electric Motors, the inrush current results from the very small impedance of the stator windings at zero speed, with the result that power consumption is greatest just at the initial start-up moment. It is only as the speed increases, with the advent of the counter electromotive force, that the effective current begins to drop to the operating value. In the case of electronic devices, such as switching power supplies or converters, the current spike is often associated with the charging of the input capacitors and the initialisation of the control circuits.

Controlling the inrush current is crucial to ensure the longevity and reliability of both the device itself and the power supply infrastructure. An excessive current pulse can lead to damage to semiconductor components, mechanical stresses, triggering of overcurrent protection or deterioration of the power grid performance. Others are therefore used in practice to limit the inrush current, such as soft-start, precharging by resistance, phase control or the use of inverters.

An accurate analysis of inrush current is important in the design of electrical installations, the selection of fuses and circuit breakers, as well as in the context of energy management and fault prevention in industrial automation and emergency power systems.

Transfer Multisort Elektronik (TME) is one of the world’s largest global distributors of electronic components, electrotechnical parts, workshop equipment, and industrial automation. The catalog includes over 1,500,000 products from 1,300 leading manufacturers. TME’s modern logistics centers in Łódź and Rzgów (Poland), with a combined area of over 40,000 m², ship nearly 6,000 packages daily to customers in more than 150 countries.

TME also invests in the development of knowledge and skills of young engineers and electronics enthusiasts through the TME Education project, and supports the tech community by organizing the TechMasterEvent series, promoting innovation and experience exchange.