+1 500 000 products in offer

7000 packages per day

+300 000 clients from 150 countries

Quick Buy Favourites
Cart

Sudo - definition

Sudo (short for 'superuser do') is a system tool used on Unix and Linux operating systems that allows a user to execute a command with the privileges of another user, by default superuser (root), without permanently changing the session context. This mechanism provides an access control mechanism based on the principle of least privilege, reducing the need to log in directly as administrator and minimising the risk of unauthorised system changes or accidental system damage.

The operation of sudo is based on verification of a user's identity based on their own password (or, in special configurations, without a password) and the rules defined in the /etc/sudoers configuration file. This file defines which users or groups are allowed to execute certain commands with elevated privileges and under what conditions. In more advanced configurations, it is possible to specify time limits, applicable hosts or permissible commands.

Sudo also introduces mechanisms for logging (logging) every attempt to execute a command, which increases the auditability of administrative operations and makes it possible to monitor potential security violations. From a technical point of view, sudo not only allows the execution of a single command, but can also pass environment variables and allow delegation of privileges in a limited and fully controlled manner.

In multi-user environments, sudo is an indispensable tool for managing operational security, enabling the effective distribution of administrative privileges without revealing the root account password. The use of sudo, together with an appropriate access policy, significantly reduces the risk of privilege escalation by unauthorised persons and enables operations to comply with the security and audit policies required in professional IT environments. In modern operating systems, sudo is often integrated with configuration management automation Tools and external authentication systems such as LDAP or Kerberos, further strengthening its role in privilege management.

Transfer Multisort Elektronik (TME) is one of the world’s largest global distributors of electronic components, electrotechnical parts, workshop equipment, and industrial automation. The catalog includes over 1,500,000 products from 1,300 leading manufacturers. TME’s modern logistics centers in Łódź and Rzgów (Poland), with a combined area of over 40,000 m², ship nearly 6,000 packages daily to customers in more than 150 countries.

TME also invests in the development of knowledge and skills of young engineers and electronics enthusiasts through the TME Education project, and supports the tech community by organizing the TechMasterEvent series, promoting innovation and experience exchange.