+1 500 000 products in offer
7000 packages per day
+300 000 clients from 150 countries
Yes, the Raspberry Pi - especially version 5 - can replace a desktop computer, but only in certain scenarios and for a certain user profile. It is not a full-fledged replacement for everyone, but in many cases it can meet the needs of the everyday user, especially if they accept certain compromises.
The Raspberry Pi 5 is the most advanced version of this miniature computer. The Cortex-A76 processor used, clocked at 2.4 GHz, and up to 16 GB of LPDDR4X RAM have significantly increased its capabilities over its predecessors. The new RP1 south bridge relieves the processor of I/O tasks (e.g. USB and SD card handling), which improves system responsiveness. In practice, this means that the Raspberry Pi 5 handles internet browsing, online documents, text editing or light office applications very well. In tests with multiple open tabs in the browser, the difference in fluidity compared to a classic computer is difficult to notice.
The Raspberry Pi mainly uses Linux-based systems - Raspberry Pi OS is officially recommended, but Ubuntu, Twister OS or specialised versions for multimedia tasks (LibreELEC) are also available. There is no native support for the full version of Windows, and the available solutions (e.g. Windows on ARM) have significant limitations, e.g. no graphics controllers with full hardware support. It is therefore important that the user is ready to work in a Linux environment, which may require adapting to new Tools and ways of managing the system.
The Raspberry Pi 5 handles 1080p and even 4K video playback well, although the latter may require optimisation and proper cooling. For games, it works well as an emulator for older consoles (e.g. NES, SNES, PSP), but will not cope with AAA games or demanding 3D graphics. The main limitation in graphics applications remains the integrated GPU, which, although newer (VideoCore VII), is not up to par with even entry-level graphics cards in desktop PCs.
For the Raspberry Pi 5 to operate stably and efficiently, a suitable power supply (27 W) and active cooling are required. The lack of a fan can result in overheating and so-called "throttling". the lack of a fan can result in overheating and so-called throttling, i.e. performance degradation due to high temperatures. Additionally, the lack of built-in memory forces the use of a microSD card or an external SSD via the PCIe connector. Despite its small size, with the addition of cooling, Enclosures and peripherals, the Raspberry Pi is no longer as compact as the board itself suggests.
For a user with basic needs - a browser, mail, documents or YouTube - the Raspberry Pi 5 can be a fully fledged computer. It is well suited for students, students, people learning programming or users looking for a power-efficient solution for everyday work. However, it will not be a satisfactory solution for those expecting to run advanced applications, video editing, computer games or a professional graphics environment.
The Raspberry Pi 5 is a powerful, state-of-the-art device that can replace a desktop computer - provided the user's requirements are moderate. It performs very well in educational and office applications or as an internet computer. However, those accustomed to a Windows environment, requiring high computing power or professional Tools may feel limited. It is always advisable to tailor the hardware to real needs. In this case, the Raspberry Pi 5 becomes a functional computer, but not a universal one.
Buy Raspberry Pi minicomputers
Transfer Multisort Elektronik (TME) is one of the world’s largest global distributors of electronic components, electrotechnical parts, workshop equipment, and industrial automation. The catalog includes over 1,500,000 products from 1,300 leading manufacturers. TME’s modern logistics centers in Łódź and Rzgów (Poland), with a combined area of over 40,000 m², ship nearly 6,000 packages daily to customers in more than 150 countries.
TME also invests in the development of knowledge and skills of young engineers and electronics enthusiasts through the TME Education project, and supports the tech community by organizing the TechMasterEvent series, promoting innovation and experience exchange.