+1 500 000 products in offer
7000 packages per day
+300 000 clients from 150 countries
Yes, the Raspberry Pi is an excellent tool for learning programming, whether you are a beginner or a more advanced user. It combines a full-fledged operating system with the ability to work directly with physical hardware, making it unique in computer science education.
Raspberry Pi is a single board computer that runs a Linux operating system (usually Raspberry Pi OS) and offers a full development environment. This means that the user can write, run and test their own code straight away, using the same Tools that are used in a professional working environment. The built-in operating system includes pre-installed development environments such as Thonny IDE (for Python) or Geany (for C/C++), as well as support for many languages, including Python, C, C++, JavaScript, Scratch, Java and Bash. In addition, it is possible to install tools for creating web applications, working with databases or learning artificial intelligence. Python - a language particularly recommended for beginners - is deeply integrated into the Raspberry Pi OS, and its syntax and the availability of libraries enable even people with no previous programming experience to get started quickly.
What sets the Raspberry Pi apart from ordinary computers is its access to physical GPIO (General Purpose Input/Output) pins, which allow direct control of electronic components. As a result, learning to program is not limited to writing code in a terminal, but has a real, tangible impact on the operation of devices - Diodes, motors, sensors, screens or Relays. This is called 'physical computing'. physical computing, or physical programming, which combines computer science with electronics and mechanics. The user learns not only the syntax of the programming language, but also the principles of embedded devices and systems, which is crucial in areas such as robotics, IoT (Internet of Things) or Industrial Robotics.
The Raspberry Pi was designed with education in mind. Thanks to this there are a huge number of free courses, projects and training materials available online in many languages. The Raspberry Pi Foundation also runs its own education platform and starter kits, which include step-by-step instructions, electronic components and lesson plans. For beginners, a huge advantage is the low price of the device, the ability to reset the system in case of errors and the support of a huge community through forums and discussion groups where users share dozens of examples of finished projects.
With the Raspberry Pi, you can learn the basics of programming through simple scripts and then move on to building your own applications, controlling devices, creating websites and even data analysis and simple machine learning algorithms. The Pi 4 or Pi 5 model also allows you to work with low-level languages (such as C) and environments like Docker or Node.js, which opens the way to more advanced software engineering.
Transfer Multisort Elektronik (TME) is one of the world’s largest global distributors of electronic components, electrotechnical parts, workshop equipment, and industrial automation. The catalog includes over 1,500,000 products from 1,300 leading manufacturers. TME’s modern logistics centers in Łódź and Rzgów (Poland), with a combined area of over 40,000 m², ship nearly 6,000 packages daily to customers in more than 150 countries.
TME also invests in the development of knowledge and skills of young engineers and electronics enthusiasts through the TME Education project, and supports the tech community by organizing the TechMasterEvent series, promoting innovation and experience exchange.