+1 500 000 products in offer
7000 packages per day
+300 000 clients from 150 countries
Yes, the Raspberry Pi supports RAID disk arrays, but only in software form. This means it doesn't have a hardware RAID controller, but can create arrays using the operating system and appropriate Linux Tools such as mdadm.
RAID (Redundant Array of Independent Disks) is a way of combining multiple disks into a single logical unit with certain characteristics, e.g. greater speed, reliability or capacity. On the Raspberry Pi, as on most consumer devices, there is no physical (hardware) RAID controller, so configuration is purely software-based, within the Linux operating system. The most commonly used variants are RAID 1 (mirror), which automatically copies data to two drives, or RAID 0 (striping), which increases performance but does not provide redundancy. In more advanced configurations, RAID 5 or RAID 10 can also be built, but this requires more media and proper power and cooling management. To support RAID on the Raspberry Pi, the most common tool used is mdadm, which allows the creation, monitoring and reconfiguration of arrays in a Linux environment. Configuration is done manually via a terminal, but once set up correctly, the system recognises the array as a single virtual disk, accessible to the user and applications.
The Raspberry Pi 4 only supports USB 3.0 ports for connecting external drives. In practice, this means that all drives are connected to a single USB bus, which can be a bottleneck under heavy I/O loads, especially in more complex arrays or when multiple services are accessed simultaneously. On the Raspberry Pi 5, the situation is improved thanks to the presence of PCIe 2.0 x1 interfaces, it is possible to connect NVMe drives or SATA controllers using HAT Adapters. This significantly increases the throughput and reliability of the system and thus improves the efficiency of RAID operation. The NVMe-enabled Raspberry Pi 5 becomes a viable platform for building a high-performance, low-power file server with data redundancy, e.g. for home or small business applications. Note that system RAID does not provide full resilience to failures, such as power loss during synchronisation or data corruption at the logical level. Therefore, in critical applications it is always advisable to use additional backup strategies and to use UPS (uninterruptible power supplies).
Transfer Multisort Elektronik (TME) is one of the world’s largest global distributors of electronic components, electrotechnical parts, workshop equipment, and industrial automation. The catalog includes over 1,500,000 products from 1,300 leading manufacturers. TME’s modern logistics centers in Łódź and Rzgów (Poland), with a combined area of over 40,000 m², ship nearly 6,000 packages daily to customers in more than 150 countries.
TME also invests in the development of knowledge and skills of young engineers and electronics enthusiasts through the TME Education project, and supports the tech community by organizing the TechMasterEvent series, promoting innovation and experience exchange.