+1 500 000 products in offer

6000 packages per day

+300 000 clients from 150 countries

Quick Buy Favourites
Cart

Microcontroller - definition

Microcontroller is an integrated digital circuit that incorporates a central processing unit (CPU), memory, and input/output interfaces, designed to control electronic devices and execute tasks in embedded systems. It functions as a self-contained computer system within a single package, capable of running programs stored in its internal memory. Unlike traditional microprocessors, microcontrollers are optimized for low power consumption, simplicity of operation, and seamless interaction with sensors, converters, and actuators.

A microcontroller typically consists of an arithmetic logic unit (ALU), RAM for data storage,, Flash memory for program storage, and a variety of digital and analog peripherals such as timers, analog-to-digital converters (ADCs), and communication interfaces like UART, SPI, and I²C. It also includes clock generation circuits and power management units. These built-in components enable the microcontroller to autonomously process data, respond to environmental signals, and control processes without the need for external control hardware.

Microcontrollers are widely used across numerous fields, including industrial automation, measurement systems, consumer electronics, automotive electronics, medical devices, smart building systems, and many other technical domains. Selection of a microcontroller depends on available hardware resources, architecture (e.g., 8-, 16-, or 32-bit), processor core type (e.g., ARM Cortex-M, AVR, PIC), and the specific requirements of the target application. Programming is typically performed in low-level languages such as C or assembly, using dedicated development environments and hardware programmers.

The key advantages of microcontrollers include their compact form factor, low unit cost, and ability to operate in real-time, making them fundamental components of modern control and automation systems. Their importance continues to grow with the advancement of miniaturization and the increasing demand for smart, energy-efficient embedded solutions.

Transfer Multisort Elektronik (TME) is one of the world’s largest global distributors of electronic components, electrotechnical parts, workshop equipment, and industrial automation. The catalog includes over 1,500,000 products from 1,300 leading manufacturers. TME’s modern logistics centers in Łódź and Rzgów (Poland), with a combined area of over 40,000 m², ship nearly 6,000 packages daily to customers in more than 150 countries.

TME also invests in the development of knowledge and skills of young engineers and electronics enthusiasts through the TME Education project, and supports the tech community by organizing the TechMasterEvent series, promoting innovation and experience exchange.

READ ALSO