+1 500 000 products in offer

7000 packages per day

+300 000 clients from 150 countries

Quick Buy Favourites
Cart

Dielectric - definition

A dielectric is a material that poorly conducts electric current but effectively stores electric charge in the presence of an electrostatic field. It is characterized by a very high electrical resistivity and a low concentration of free charge carriers, meaning that under normal conditions, no significant current flows through it. Dielectric properties arise from the atomic structure and the ability of molecules to become polarized when exposed to an external electric field, resulting in the formation of internal dipoles.

In technical systems, dielectrics serve as insulators, separating conductive elements and preventing unwanted current flow. Their application is especially important in the design of capacitors, where a dielectric material placed between the electrodes increases the device’s ability to store electrical energy. The performance of electronic components, cables, high-voltage systems, and microwave devices depends on key dielectric parameters such as permittivity, dielectric strength, and loss factor.

Dielectrics can be natural or synthetic and may exist in various physical states—including solids, liquids, or gases. The selection of an appropriate dielectric material depends on application-specific requirements such as operating temperature range, chemical resistance, durability, and the influence of signal frequency. In advanced electronic technologies, dielectrics play a crucial role in the miniaturization and enhancement of integrated circuit performance, as well as in the protection of circuits against electrical breakdown.

Transfer Multisort Elektronik (TME) is one of the world’s largest global distributors of electronic components, electrotechnical parts, workshop equipment, and industrial automation. The catalog includes over 1,500,000 products from 1,300 leading manufacturers. TME’s modern logistics centers in Łódź and Rzgów (Poland), with a combined area of over 40,000 m², ship nearly 6,000 packages daily to customers in more than 150 countries.

TME also invests in the development of knowledge and skills of young engineers and electronics enthusiasts through the TME Education project, and supports the tech community by organizing the TechMasterEvent series, promoting innovation and experience exchange.

READ ALSO