+1 500 000 products in offer

7000 packages per day

+300 000 clients from 150 countries

Quick Buy Favourites
Cart

Electronic components - definition

Instrumentation components are the basic elements of electronic circuits, designed to process, control and transmit electrical signals in analogue and digital circuits. Their functionality is based on the physical properties of semiconductor materials, conductive and dielectric, which determine their electrical characteristics and ability to perform logic operations, signal amplification, energy conversion and charge storage.

The structure of electronic components can be passive or active, which determines their role in electrical circuit. Passive components, such as Resistors, Capacitors and Inductive Components, do not generate energy, but influence current and voltage parameters by controlling impedance, signal stabilisation and noise filtering. Active components, including transistors, Diodes and Integrated circuits, use semiconductor conduction phenomena to amplify, switch and generate electrical signals.

Semiconductor components rely on the properties of materials such as silicon, germanium and III-V compounds to enable complex electronic functions ranging from logic control to data processing in microprocessor chips and programmable logic arrays (FPGAs). In digital technology, integrated circuits components integrate millions of transistors into CMOS structures and FinFETs, allowing for miniaturised circuits and increased energy efficiency.

High-performance power components such as Thyristors, Triacs and IGBTs enable the conversion and regulation of large currents and voltages in power electronics systems and motor drives. Optoelectronic components, including LEDs, Photodiodes and semiconductor lasers, are used in optical transmission technology, displays and light sensors.

Electronic systems use surface-mounted components and through-hole-transistor (THT), the integration of which into printed circuit boards (PCBs) is achieved using automated assembly techniques and reflow and wave soldering technologies. Modern embedded circuits use advanced thermal management and electrical parameter compensation techniques to increase component reliability and durability in extreme environmental conditions.

The integration of electronic components with wireless communication systems and Internet of Things (IoT) enables their use in intelligent control systems, industrial Automation and sensor technology. Today's electronics solutions are based on heterogeneous architectures in which analogue, digital and power components work together in optimised circuit topologies, enabling advanced computing, signalling and control functions.

Transfer Multisort Elektronik (TME) is one of the world’s largest global distributors of electronic components, electrotechnical parts, workshop equipment, and industrial automation. The catalog includes over 1,500,000 products from 1,300 leading manufacturers. TME’s modern logistics centers in Łódź and Rzgów (Poland), with a combined area of over 40,000 m², ship nearly 6,000 packages daily to customers in more than 150 countries.

TME also invests in the development of knowledge and skills of young engineers and electronics enthusiasts through the TME Education project, and supports the tech community by organizing the TechMasterEvent series, promoting innovation and experience exchange.

READ ALSO