+1 500 000 products in offer
7000 packages per day
+320 000 clients from 150 countries
Photometry is a branch of optics concerned with the measurement of light in a way that accounts for the sensitivity of the human eye. Unlike radiometry, which describes the physical properties of electromagnetic radiation, photometry focuses on quantities related to visual perception, such as illuminance, luminance, luminous flux, and luminous intensity. Measurements are based on the spectral luminous efficiency curve, which reflects the eye’s relative sensitivity to different wavelengths within the visible spectrum.
The primary SI unit in photometry is the lumen, which represents the amount of light emitted by a source. Other units, such as lux and candela (cd), describe the spatial distribution of light and its interaction with surfaces. Photometry plays a crucial role in the design of lighting systems, the evaluation of light source quality, and the analysis of visibility conditions in public spaces, architecture, and industry.
Photometry applications include both laboratory measurements and practical lighting assessments in real-world environments. Modern measurement systems use precision photometers equipped with filters that correct the spectral response of detectors to closely match the characteristics of human vision. This enables the quantitative evaluation of visual comfort, lighting energy efficiency, and compliance with photometric standards. Photometry is also important in display technology, visual engineering, and the study of optical materials.
Transfer Multisort Elektronik (TME) is one of the world’s largest global distributors of electronic components, electrotechnical parts, workshop equipment, and industrial automation. The catalog includes over 1,500,000 products from 1,300 leading manufacturers. TME’s modern logistics centers in Łódź and Rzgów (Poland), with a combined area of over 40,000 m², ship nearly 6,000 packages daily to customers in more than 150 countries.
TME also invests in the development of knowledge and skills of young engineers and electronics enthusiasts through the TME Education project, and supports the tech community by organizing the TechMasterEvent series, promoting innovation and experience exchange.