+1 500 000 products in offer

7000 packages per day

+320 000 clients from 150 countries

Quick Buy Favourites
Cart

Clectromagnetic radiation - definition

Electromagnetic radiation is a form of energy that propagates through space as a result of the mutual variations of electric and magnetic fields. Electromagnetic waves are generated by the accelerated motion of electric charges and do not require a material medium for propagation—they can travel through a vacuum, which distinguishes them from mechanical waves. A defining feature of electromagnetic radiation is that the electric and magnetic fields are perpendicular to each other and to the direction of wave propagation.

This radiation spans a wide range of frequencies—from radio waves with wavelengths of several kilometers, through microwaves, infrared radiation, visible light, and ultraviolet radiation, to high-energy X-rays and gamma rays. The differences between these types of radiation lie primarily in their wavelength, frequency, and quantum energy, which directly affect their interaction with matter and technological applications.

From the perspective of quantum physics, electromagnetic radiation can be described both as a wave and as a stream of particles called photons, illustrating wave-particle duality. A photon is a massless elementary particle whose energy depends on the frequency of the radiation, as described by Planck’s relation. This dual nature allows electromagnetic radiation to be modeled using both Maxwell’s wave equations and quantum theory.

Electromagnetic radiation plays a fundamental role in nature and technology. It serves as a carrier of information, a source of heat, a diagnostic tool, and the basis for the operation of communication systems, optical devices, radars, and medical imaging methods. The interaction of electromagnetic waves with matter depends on the structure of the material and the radiation frequency—it can result in absorption, reflection, refraction, diffraction, or ionization, all of which are exploited across various scientific and engineering disciplines.

Transfer Multisort Elektronik (TME) is one of the world’s largest global distributors of electronic components, electrotechnical parts, workshop equipment, and industrial automation. The catalog includes over 1,500,000 products from 1,300 leading manufacturers. TME’s modern logistics centers in Łódź and Rzgów (Poland), with a combined area of over 40,000 m², ship nearly 6,000 packages daily to customers in more than 150 countries.

TME also invests in the development of knowledge and skills of young engineers and electronics enthusiasts through the TME Education project, and supports the tech community by organizing the TechMasterEvent series, promoting innovation and experience exchange.

READ ALSO