+1 500 000 products in offer

7000 packages per day

+300 000 clients from 150 countries

Quick Buy Favourites
Cart

Can Batteries corrode?

Yes, batteries can corrode, especially if they are left in appliances for long periods or are damaged. This corrosion is the result of electrolyte leakage, which reacts with the metal parts and the air, forming a corrosive deposit.

Why do Batteries corrode?

In most cases corrosion occurs in zinc and-carbon batteries and alkaline, and alkaline batteries can leak over time. The electrolyte contained in such batteries is usually potassium hydroxide or ammonium chloride - chemically reactive substances. When a battery is discharged or stored in poor conditions (e.g. in high humidity), can lead to enclosures leak, and electrolyte starts to leak out. Contact with air and metallic parts results in the appearance of a white or bluish deposit, which is a sign of corrosion.

Is it dangerous for batteries to corrode?

Yes, but to a limited extent. Although corrosion of Batteries does not cause violent chemical reactions, but substances contained in the spill can be corrosive to the skin and can damage electronics. It is therefore very important, not to ignore visible signs of battery damage and to regularly check the condition of battery-powered devices.

How to clean up a battery leak safely?

If you notice corrosion in a device, first of all unplug the device and remove the Batteries. Then wear protective gloves - even homemade latex or nitrile gloves - to avoid contact with the electrolyte. To neutralise the deposits, it is best to use a solution of vinegar or lemon juice, which reacts with alkaline electrolyte residues, dissolving them. It is sufficient to gently wipe the affected areas with a cotton bud or a cloth soaked in the solution. After cleaning, dry the area and check the following, that there is no permanent damage to the tracks, contacts or plastic parts. If the metal contacts are more deeply damaged, they may need to be sanded or even replaced.

IMPORTANT: Do not attempt to use the device, before it has been thoroughly cleaned and checked.

How to prevent corrosion of Batteries?

The best way is to regularly check the condition of batteries, especially in devices that are used infrequently. Batteries should also be removed from devices, remove batteries from devices that are to be stored for long periods. Using branded cells and avoiding overcharging or completely discharging them also reduces the risk of chemical damage.

IMPORTANT: If you are not sure, whether a device is still usable after a battery leak, consult a qualified service technician or electronics technician. Improper cleaning may aggravate damage or lead to further corrosion.

Transfer Multisort Elektronik (TME) is one of the world’s largest global distributors of electronic components, electrotechnical parts, workshop equipment, and industrial automation. The catalog includes over 1,500,000 products from 1,300 leading manufacturers. TME’s modern logistics centers in Łódź and Rzgów (Poland), with a combined area of over 40,000 m², ship nearly 6,000 packages daily to customers in more than 150 countries.

TME also invests in the development of knowledge and skills of young engineers and electronics enthusiasts through the TME Education project, and supports the tech community by organizing the TechMasterEvent series, promoting innovation and experience exchange.

READ ALSO