+1 500 000 products in offer

7000 packages per day

+300 000 clients from 150 countries

Quick Buy Favourites
Cart

How does battery charging work?

Charging a battery involves reversing the chemical reaction that occurred when the battery was discharged - that is, providing electricity to build up the charge inside the cell again

The chemical process in a secondary cell

Batteries that can be recharged are known as. Secondary cells - as opposed to disposable primary cells. The most common types of rechargeable batteries are lithium-ion, nickel-metal hydride (NiMH) and lead-acid. In each of these cases, charging is carried out by applying voltage from an external source (Chargers), which forces a current flow opposite to the direction of discharge.This current flow causes the ions inside the Batteries to move back to their original electrodes, restoring their responsiveness. As a result, the cell is again able to yield energy during the next discharge cycle.

The role of the battery charge controller

In modern devices, the charging process is supervised by a control system (the so-called BMS - Battery Management System). Its task is to regulate voltage, charging current and temperature to prevent overheating, overcharging and cell damage. This is especially true for lithium-ion batteries, which are highly efficient but also sensitive to improper operating conditions.Rechargeable Batteries (e.g. automotive batteries) use staged charging, which reduces the current as they approach full charge. This helps to **extend battery life and minimise energy loss

Effectiveness and durability

Not every battery tolerates a large number of charge cycles well. Each cycle is electrochemical wear and tear on the internal materials, which deteriorates the performance of the cell over time. Rechargeable Batteries are therefore designed with a specific number of cycles in mind - for lithium-ion, this can be several hundred to several thousand.It is also important to not lead to extreme states of charge - neither to full discharge nor to overcharge. Batteries operate optimally in the so-called safe voltage zone.

IMPORTANT: If you are unsure about how to charge a particular type of battery, it is advisable to read the manufacturer's recommendations or consult a technician.

Transfer Multisort Elektronik (TME) is one of the world’s largest global distributors of electronic components, electrotechnical parts, workshop equipment, and industrial automation. The catalog includes over 1,500,000 products from 1,300 leading manufacturers. TME’s modern logistics centers in Łódź and Rzgów (Poland), with a combined area of over 40,000 m², ship nearly 6,000 packages daily to customers in more than 150 countries.

TME also invests in the development of knowledge and skills of young engineers and electronics enthusiasts through the TME Education project, and supports the tech community by organizing the TechMasterEvent series, promoting innovation and experience exchange.

READ ALSO