+1 500 000 products in offer
7000 packages per day
+300 000 clients from 150 countries
The Arduino's bootloader is a small program stored in the microcontroller's memory, which allows code to be uploaded from a computer to the board without the need for specialised programming hardware. Although technically you can do without it, its presence is crucial to the simplicity of the Arduino, especially in educational and prototyping applications.
The bootloader is a piece of software stored in the microcontroller's Flash memory, usually at the very end of the microcontroller. It starts automatically when the board is restarted, i.e. when the board is connected to the power supply, when the RESET button is pressed or when the transmission from the Arduino IDE starts. For a few seconds, the bootloader listens for data sent by the computer, waiting for commands that may contain new code to be uploaded. If there is an attempt to upload a program within this short time window, the bootloader receives the data and writes it to program memory. If not - transfers control to the existing user program, which starts executing normally from the setup() function. This mechanism allows the user to conveniently update the program via USB, without the need for an external ISP (In-System Programmer) or opening the Enclosures of the device.
The main advantage of the bootloader is to simplify the programming process. The Arduino was designed from the beginning with non-technical users in mind, i.e. students, teachers, hobbyists. With the bootloader, all you need is a USB cable and the Arduino IDE to upload new code to the device. Without this mechanism, separate tools and protocols would have to be used, which are much more difficult to use and require additional hardware. In addition, the bootloader allows to easily distribute Arduino boards ready to use with a pre-programmed boot system, ready to accept any user sketch.
From the point of view of microcontroller operation - no, the bootloader is not absolutely necessary. It can be removed completely and programs can be uploaded directly via the ISP connector, a practice used in industrial or performance-optimised designs. Deleting the bootloader allows you to reclaim a chunk of Flash memory (e.g. 512 bytes to 2KB) and reduce program boot time. However, for the typical Arduino user, the presence of the bootloader is a huge convenience. If it is damaged or accidentally overwritten, it is possible to restore it, e.g. using a second Arduino board acting as an ISP Programmer.
Transfer Multisort Elektronik (TME) is one of the world’s largest global distributors of electronic components, electrotechnical parts, workshop equipment, and industrial automation. The catalog includes over 1,500,000 products from 1,300 leading manufacturers. TME’s modern logistics centers in Łódź and Rzgów (Poland), with a combined area of over 40,000 m², ship nearly 6,000 packages daily to customers in more than 150 countries.
TME also invests in the development of knowledge and skills of young engineers and electronics enthusiasts through the TME Education project, and supports the tech community by organizing the TechMasterEvent series, promoting innovation and experience exchange.