+1 500 000 products in offer
7000 packages per day
+300 000 clients from 150 countries
Yes, some damage to Memory Cards can be 'fixed', but the effectiveness depends on the type of fault. It is possible to restore card operation in the case of logical errors, while physical damage and memory controller failures usually require specialist intervention or end in permanent data loss.
The most common type of problem is logical damage, i.e. data structure errors on the card resulting from improper disconnection, power failure or write errors. In such cases, the card can be detected by the system, but e.g. requires formatting or reports access errors. In Windows, you can use the Tools CHKDSK, which scans the file system and repairs any errors detected. An example command on the command line is chkdsk X: /f, where 'X' is the letter assigned to the card. Alternatively, applications such as H2testw, SD Formatter or partition restore programs can help. In many cases, the card regains full functionality and the data can be saved. However, if the operating system no longer recognises the card, the effectiveness of such tools is limited.
Mechanical damage, such as broken contacts, bent enclosure or flooding, is not suitable for self-repair. In the case of microSD cards, due to their small size and compact design, any tampering may worsen the technical condition. Failures of the Memory Controller, the integrated circuit that manages the writing and reading of data, are often invisible to the user but manifest themselves as a 'dead card'. In such cases, data recovery is only possible in a specialised laboratory that can read the contents of flash NAND memory chips directly, bypassing the faulty controller.
If the card is not working properly but is visible in the system, quick formatting can restore its functionality. Please note that formatting does not repair physical damage, but only restores the logical structure of the media. Before formatting, it is a good idea to make a backup as long as the data can still be accessed. In the case of encrypted cards (e.g. on an Android phone), formatting removes the encryption key, which means permanent data loss. If in doubt, especially when working with important files, it is worth consulting a data recovery service rather than taking the risk of losing the contents of the card.
Transfer Multisort Elektronik (TME) is one of the world’s largest global distributors of electronic components, electrotechnical parts, workshop equipment, and industrial automation. The catalog includes over 1,500,000 products from 1,300 leading manufacturers. TME’s modern logistics centers in Łódź and Rzgów (Poland), with a combined area of over 40,000 m², ship nearly 6,000 packages daily to customers in more than 150 countries.
TME also invests in the development of knowledge and skills of young engineers and electronics enthusiasts through the TME Education project, and supports the tech community by organizing the TechMasterEvent series, promoting innovation and experience exchange.