+1 500 000 products in offer
7000 packages per day
+300 000 clients from 150 countries
Memory Cards should be formatted when there are write errors, slowdowns, problems reading data or after using a new card in a device for the first time.Regular formatting also keeps the data structure in good shape and extends the life of the media.
Formatting is the process of creating a logical structure that allows files to be stored on the card. Unlike simple data deletion, which merely marks files as "invisible", formatting actually resets the file system, thus eliminating errors and data fragmentation. This is particularly important in devices that record video or perform serial recording operations, e.g. recorders, cameras or car cameras.
It is recommended to format a new card before using for the first time in a specific device. This allows you to prepare a file system that is compatible with your hardware requirements, preventing compatibility problems. Another situation is changing the device, for example moving the card between a camera and a computer or phone. Each device may use slightly different storage parameters, so it is a good idea to do a formatting before prolonged use in a new environment. The card should also be formatted regularly in write-intensive devices, such as cameras, car cameras or CCTV cameras. In such applications, even a weekly formatting procedure is recommended to avoid file system errors and ensure stable operation. If the card starts to show unusual symptoms, such as e.g. disappearing files, inability to write, error messages or a formatting requirement, this is a sign that the data structure may have been corrupted. In this case, formatting is a form of logical 'repair' of the card, although it will not solve physical problems such as flash memory corruption.
Contrary to common myths, frequent formatting does not shorten the life of Memory Cards, as long as it is done correctly and is not combined with an excessive number of full data overwrites. A quick formatting, i.e. one that only removes the file headers, is considered safe and recommended in most cases. Formatting is not only a way of deleting data, but above all a maintenance tool to ensure the stability and full performance of the Memory Cards.
Transfer Multisort Elektronik (TME) is one of the world’s largest global distributors of electronic components, electrotechnical parts, workshop equipment, and industrial automation. The catalog includes over 1,500,000 products from 1,300 leading manufacturers. TME’s modern logistics centers in Łódź and Rzgów (Poland), with a combined area of over 40,000 m², ship nearly 6,000 packages daily to customers in more than 150 countries.
TME also invests in the development of knowledge and skills of young engineers and electronics enthusiasts through the TME Education project, and supports the tech community by organizing the TechMasterEvent series, promoting innovation and experience exchange.