+1 500 000 products in offer

7000 packages per day

+300 000 clients from 150 countries

Quick Buy Favourites
Cart

Why does the memory card get damaged?

Memory Cards fail most often due to wear and tear of flash memory cells, logical errors, mechanical damage or electrical disturbances. Any of these factors can lead to data loss, performance degradation or complete media immobilisation.

Technological wear and tear of flash memory

Memory Cards SD and microSD are based on NAND flash memory, which has a limited number of write and erase cycles. Each memory cell can only be written to and erased a certain number of times, after which it loses its ability to store data. This phenomenon, known as wear-out, is inevitable and progresses faster in low-quality or heavily used cards, e.g. in car recorders, surveillance cameras or drones. Symptoms of wear-out include slower writing, errors occurring, loss of files or the card going into read-only mode.

Memory card logical failures

The most common problems include file system errors, which occur as a result of improper disconnection of the card from the device, interrupted writing, power surges or viruses. Such damage leads to a situation where the card is visible but inaccessible, reports errors or requires formatting. Logical failures do not yet mean the loss of the media itself. They can often be repaired using diagnostic tools such as chkdsk (Windows command), SD Formatter or partition repair software.

Electronics failure and electrical faults

Memory Cards contain a controller, which is a microprocessor responsible for managing writing, reading and communication with the device. Controller failure can result in a sudden failure to detect the card, unstable operation or complete media lock-up. Often such damage is irreversible and requires the intervention of a service that recovers data directly from the NAND. An additional risk is surges and voltage spikes, which can damage the electronics on the card, especially when connected to faulty USB readers, cheap adapters or unstable Power Supplies.

Mechanical damage to Memory Cards

Broken casing, cracked Laminates, scratches or corrosion of contacts are typical mechanical failures. These particularly affect microSD cards, which are more susceptible to physical strain due to their small size. Any bending, flexing or soiling can damage the data line or voltage, preventing the card from continuing to function. Memory Cards, despite their simplicity, are complex electronic devices. Their durability depends on both the quality of manufacture and the way they are used.

Transfer Multisort Elektronik (TME) is one of the world’s largest global distributors of electronic components, electrotechnical parts, workshop equipment, and industrial automation. The catalog includes over 1,500,000 products from 1,300 leading manufacturers. TME’s modern logistics centers in Łódź and Rzgów (Poland), with a combined area of over 40,000 m², ship nearly 6,000 packages daily to customers in more than 150 countries.

TME also invests in the development of knowledge and skills of young engineers and electronics enthusiasts through the TME Education project, and supports the tech community by organizing the TechMasterEvent series, promoting innovation and experience exchange.

READ ALSO