+1 500 000 products in offer

7000 packages per day

+300 000 clients from 150 countries

Quick Buy Favourites
Cart

Why does the memory card stop working?

Memory Cards typically cease to function as a result of flash memory wear, logical file system damage, controller failure or mechanical physical damage. Any of these causes can lead to a sudden loss of data access or a complete unresponsiveness of the device to the inserted card.

Memory cell wear

NAND flash memory technology, as used in SD and microSD cards, is based on a limited number of write and erase cycles. With use, the cells holding the data gradually lose their ability to write stably until the card stops working or goes into read-only mode. This phenomenon is typical of media used for a long time in write-intensive devices such as video recorders or surveillance cameras.

Logical errors and corrupted file system

Improper card disconnection, interrupted recording, software errors or malware infection can lead to damage to the logical data structure. In this case, the card may be visible by the system, but requests formatting, reports missing files or displays errors. It is sometimes possible to repair it with Tools such as chkdsk or SD Formatter, but aggravated logical damage can effectively prevent further use.

Memory controller failures

Each card contains an embedded microcontroller, which manages the data flow and communication with the device. When it fails (e.g. due to an overvoltage, manufacturing defect or overheating), the card is no longer recognised and becomes inaccessible. This type of failure is often permanent and irreversible without specialist data recovery and usually marks the end of the life of the media.

Mechanical and contact damage to Memory Cards

MicroSD cards are susceptible to bending, cracking and contact damage, which can lead to communication problems with the reader. Even minor deformations or dirt can prevent the contents from being read correctly. Also, improper use of SD Adapters or Memory Cards slots in devices can accelerate wear and tear and lead to permanent failure. Memory Cards, although small in size, are complex electronic circuits that can cease to function over time and under operating conditions. Regular backups and careful use are essential measures to protect against data loss.

Transfer Multisort Elektronik (TME) is one of the world’s largest global distributors of electronic components, electrotechnical parts, workshop equipment, and industrial automation. The catalog includes over 1,500,000 products from 1,300 leading manufacturers. TME’s modern logistics centers in Łódź and Rzgów (Poland), with a combined area of over 40,000 m², ship nearly 6,000 packages daily to customers in more than 150 countries.

TME also invests in the development of knowledge and skills of young engineers and electronics enthusiasts through the TME Education project, and supports the tech community by organizing the TechMasterEvent series, promoting innovation and experience exchange.

READ ALSO