+1 500 000 products in offer

7000 packages per day

+300 000 clients from 150 countries

Quick Buy Favourites
Cart

How long does the Raspberry Pi run on battery power?

The Raspberry Pi's runtime on battery power depends on several factors, primarily the model of the device, the type of Batteries and the intensity of use, but in practice ranges from around 2 to 12 hours. The latest models, such as the Raspberry Pi 5, consume significantly more power than earlier versions and require more capacious Power Sources.

Power consumption of different Raspberry Pi models

Each Raspberry Pi model has different power requirements. The Raspberry Pi Zero W consumes just 0.5-1 W, allowing it to run for hours on a small lithium polymer battery. In contrast, the Raspberry Pi 4 consumes around 3-5 W in typical applications, and the Raspberry Pi 5 consumes up to 10-12 W under full load, e.g. when using a web browser, displaying 4K video or compiling code. This means that the newer and more powerful the model, the shorter the runtime on the same battery pack. These differences are significant and should be taken into account when designing mobile applications with the Raspberry Pi.

Calculating the Raspberry Pi's battery life

To estimate the Raspberry Pi's runtime on a battery, it is necessary to know its capacity (expressed in mAh) and its output voltage. A typical powerbank with a capacity of 10,000 mAh at 3.7 V gives approximately 37 Wh (i.e. 10 Ah × 3.7 V = 37 Wh), of which approximately 30 Wh is effectively available after conversion losses and voltage stabilisation are taken into account. If the Raspberry Pi 4 consumes 4 W on average, such a powerbank will provide power for about 7-8 hours. In the case of the Raspberry Pi 5, with a consumption of 8-10 W, this time is reduced to 3-4 hours. The Raspberry Pi Zero, on the other hand, with a consumption of around 0.5 W, can even run for more than 40 hours from the same source. In projects powered by Li-Ion or LiFePO4 rechargeable battery packs, the runtime will depend on the configuration of the cells (e.g. 2S1P, 3S2P), the capacity and the voltage converter used (step-down or buck-boost), which stabilises the voltage to the 5.1 V required by the Pi.

Optimising the Raspberry Pi's power consumption

To extend the Raspberry Pi's battery life, it is a good idea to reduce unnecessary features. You can disable Wi-Fi and Bluetooth interfaces, reduce the brightness of the screen backlight, use a version of the system without a graphical environment (e.g. Raspberry Pi OS Lite) and minimise the activity of peripherals such as cameras, sensors or USB devices. On the Raspberry Pi 5, it is also possible to limit the maximum CPU frequency and deactivate ports, which can reduce power consumption by several watts. Using Tools for power management and system load monitoring will help optimise performance according to application needs.

Typical applications of battery power

Battery power is used in mobile projects such as portable measurement stations, data acquisition systems, robots, IoT devices, field installations or wherever access to mains power is not possible. However, it is important to note that the Raspberry Pi does not have built-in charge management or battery protection - so it is worth using dedicated BMS (Battery Management System) modules or external charge controllers for battery projects.

Transfer Multisort Elektronik (TME) is one of the world’s largest global distributors of electronic components, electrotechnical parts, workshop equipment, and industrial automation. The catalog includes over 1,500,000 products from 1,300 leading manufacturers. TME’s modern logistics centers in Łódź and Rzgów (Poland), with a combined area of over 40,000 m², ship nearly 6,000 packages daily to customers in more than 150 countries.

TME also invests in the development of knowledge and skills of young engineers and electronics enthusiasts through the TME Education project, and supports the tech community by organizing the TechMasterEvent series, promoting innovation and experience exchange.

READ ALSO