+1 500 000 products in offer
7000 packages per day
+300 000 clients from 150 countries
Yes, the Raspberry Pi supports cameras and allows video streaming (both locally and over the network), provided the right components and software are selected. Newer models, such as the Raspberry Pi 4 and 5, offer enough processing power to seamlessly handle HD and even 4K video in real time.
The Raspberry Pi is equipped with dedicated camera connectors CSI (Camera Serial Interface), which allow the connection of official camera modules, e.g. Raspberry Pi Camera Module 3, HQ Camera or FLIR Infrared Cameras. On the latest Raspberry Pi 5, there are two independent CSI-2 ports, which allows two cameras to be connected at the same time and transmit from both sources. In addition to CSI cameras, it is also possible to use USB cameras, e.g. popular webcams that are automatically detected by the system as video devices (/dev/video0). Cameras of this type are convenient to use, but may have higher latency and lower quality than dedicated models. Camera support does not require specialised software, as Raspberry Pi OS includes the controllers and libraries necessary for V4L2 (Video4Linux2) cameras and support for the libcamera interface, a modern framework for managing imaging devices.
The Raspberry Pi is suitable for real-time video streaming, e.g. to transmit video from a camera over a local network or the internet. Using Tools such as FFmpeg, GStreamer, VLC, OBS (ARM version) or Motion it is possible to stream to a browser, mobile application or streaming platform. Two types of transmission are most commonly used:
Long-term streaming requires a stable power supply and good cooling, especially on the Raspberry Pi 5 where video decoding and encoding generates high temperatures. It is advisable to use active cooling and a minimum 5 A power supply. When working over Wi-Fi, transmission delays and instability can occur, so a wired connection over Ethernet is recommended for HD streaming. Streaming performance also depends on the system configuration, the type of software used and the quality of the video. It is worth mentioning that the Raspberry Pi can also act as a IP camera server or monitoring system (e.g. using MotionEye software), with the possibility of recording, motion detection and remote viewing from a browser.
Transfer Multisort Elektronik (TME) is one of the world’s largest global distributors of electronic components, electrotechnical parts, workshop equipment, and industrial automation. The catalog includes over 1,500,000 products from 1,300 leading manufacturers. TME’s modern logistics centers in Łódź and Rzgów (Poland), with a combined area of over 40,000 m², ship nearly 6,000 packages daily to customers in more than 150 countries.
TME also invests in the development of knowledge and skills of young engineers and electronics enthusiasts through the TME Education project, and supports the tech community by organizing the TechMasterEvent series, promoting innovation and experience exchange.