+1 500 000 products in offer

7000 packages per day

+300 000 clients from 150 countries

Quick Buy Favourites
Cart

Is the RP2040 (microcontroller from Raspberry Pi) a "full Raspberry Pi"?

No. The RP2040 is a microcontroller (MCU) and not a full-fledged single board computer (SBC) in the Raspberry Pi family. It should be regarded as a separate product category, designed for low-level tasks and working without a full operating system.

What is the RP2040 in practice?

The RP2040 is a chip designed by Raspberry Pi for embedded applications. It works 'close to the hardware', executing code directly on the MCU cores, typically without an operating system, possibly with lightweight runtime environments such as MicroPython or C/C++ applications. The key difference is that the RP2040 does not run a Linux-type system, nor does it have a graphics controller, HDMI interfaces or the typical multi-gigabyte RAM. Its domain is deterministic tasks: signal acquisition, precise waveform generation, sensor support and simple interfaces. This approach, which is deliberately minimalist, makes it possible to achieve very low latency and high repeatable timings.

What makes the 'full' Raspberry Pi different from the RP2040?

Full Raspberry Pi (e.g. models 4 or 5) are SBCs that run Raspberry Pi OS (Linux) and utility applications, support Displays via HDMI, offer USB ports, wired and wireless networking, and store the system and data on an SSD, NVMe or microSD card. It is a general-purpose environment - with a network stack, gigabyte memory and multitasking - designed for desktop, server and IoT software. The RP2040, meanwhile, is a microcontroller without a full OS, optimised for control and simple real-time algorithms. The documentation explicitly stresses that the RP2040 "is not a full-fledged Raspberry Pi" and is a separate product category to the SBC.

When to choose the RP2040 and when to choose the SBC Raspberry Pi

If you need simple, repeatable and fast responses to hardware events - controlling motors, reading sensors at precise intervals, generating waveforms - the RP2040 will work well as a 'real-time brain'. However, when a project requires a file system, networking, graphical interfaces, multi-threaded operation and running Linux applications, a full Raspberry Pi is the right choice. A common and very effective approach is a hybrid architecture: the Raspberry Pi's SBC is responsible for high-level logic, communications and data storage, while the RP2040 performs time-critical tasks at the signal line level. The official guide emphasises this complementarity - the RP2040 is described as a microcontroller for low-level tasks, not a substitute for an SBC computer.

Transfer Multisort Elektronik (TME) is one of the world’s largest global distributors of electronic components, electrotechnical parts, workshop equipment, and industrial automation. The catalog includes over 1,500,000 products from 1,300 leading manufacturers. TME’s modern logistics centers in Łódź and Rzgów (Poland), with a combined area of over 40,000 m², ship nearly 6,000 packages daily to customers in more than 150 countries.

TME also invests in the development of knowledge and skills of young engineers and electronics enthusiasts through the TME Education project, and supports the tech community by organizing the TechMasterEvent series, promoting innovation and experience exchange.

READ ALSO