+1 500 000 products in offer
7000 packages per day
+300 000 clients from 150 countries
Yes, the Raspberry Pi is a normal Linux host on the network, so with poor configuration it is sometimes vulnerable to attacks, especially over SSH. The risks are mainly due to default or weak passwords, an outdated system and enabled, unused services. However, a well-configured Pi is safe for practical use.
The Raspberry Pi often boots 'headless' and administration is done remotely over SSH. This is convenient, but means that the SSH port becomes a gateway to the system: if the password is predictable, an attacker can guess it using a dictionary method. The documentation highlights that the biggest mistake is leaving the default credentials (used to be 'pi/ Raspberry Pi') and not immediately changing the password and username to unique and strong ones. Raspberry Pi should be treated like any server on the internet - keep it up to date, limit service exposure and take care of password policy.
Most benefit authentication with SSH keys instead of passwords. The private key remains with the administrator and the server only accepts the corresponding public key, virtually eliminating the effectiveness of dictionary attacks. At the same time, it is worth disabling password logins and, if possible, restricting SSH to the internal network or VPN tunnel. This is complemented by regularly updating the system and running the firewall and disabling unused services, so as to minimise the attack surface. These principles are identified in the guide as essential elements of Raspberry Pi security hygiene.
In typical deployments, it is dangerous to expose SSH directly to the Internet with a password 'to remember'. It is safer to keep the Pi on the local network segment and use key-by-key access, and when remote access is required, add a layer of control such as an IP address filter or service that restricts login attempts. It's worth remembering that the Raspberry Pi OS is being actively developed, with ongoing updates fixing vulnerabilities and closing known attack vectors - an up-to-date system is a real risk reduction. The biggest enemy of security is 'leaving everything the way it works when it first starts up'
If you connect over SSH with a password, don't have your keys configured and can't remember when you last updated your system, your Pi is an easy target. Also, leaving services on that you don't use increases exposure. In headless mode, the device is sometimes administered "remotely and in the dark" for long periods of time, so discipline in updates and access control is crucial. A secure SSH configuration plus an up-to-date Raspberry Pi OS is the foundation that effectively neutralises the most common attacks in most home and small business scenarios.
Transfer Multisort Elektronik (TME) is one of the world’s largest global distributors of electronic components, electrotechnical parts, workshop equipment, and industrial automation. The catalog includes over 1,500,000 products from 1,300 leading manufacturers. TME’s modern logistics centers in Łódź and Rzgów (Poland), with a combined area of over 40,000 m², ship nearly 6,000 packages daily to customers in more than 150 countries.
TME also invests in the development of knowledge and skills of young engineers and electronics enthusiasts through the TME Education project, and supports the tech community by organizing the TechMasterEvent series, promoting innovation and experience exchange.