+1 500 000 products in offer

7000 packages per day

+300 000 clients from 150 countries

Quick Buy Favourites
Cart

Can a magnet delete data from a memory stick?

No, a magnet cannot erase data from a memory stick. This is a common myth that stems from confusion between modern storage media and old magnetic recording-based technologies. Pendrives and other flash storage devices are resistant to magnetic fields - even very strong ones.

How does flash memory work?

A flash drive uses what is known as flash memory - an electronic circuit in which data is stored as electrical charges in the gates of transistors. Each memory cell represents information by the presence or absence of a charge. This state is retained without the need for power, making flash memory a type of non-volatile memory. What is important is that flash memory does not use magnetism in any stage of writing or reading data. This means that the magnetic field - whether from a ferrite magnet, neodymium magnet or Solenoids - has no effect on the stored information.

Where did this myth come from?

The common belief of "erasing data with a magnet" has its roots in the past, when data storage media based on magnetic recording were widely used. Floppy disks, cassette tapes, VHS tapes or HDDs store information as ordered magnetic domains in a thin ferromagnetic layer. With such media, a strong magnetic field can actually remagnetise the recording layer and lead to irreversible data loss. However, no analogous phenomenon occurs with memory sticks, SD cards, SSDs and modern smartphones** - their data is stored purely electronically and not magnetically.

And what about other devices?

Magnets will not damage the processor, Integrated circuits or LCD screen either. These components are designed to be immune to external magnetic fields and do not rely on magnetic phenomena. The only exception is Hall Sensors based on the Hall effect (e.g. the digital compass in a phone), which may temporarily give erroneous readings in the presence of a magnet, but this does not erase data or damage the hardware. Once the magnet is removed and possibly calibrated, the sensor returns to correct operation.

Are there situations where a magnet can harm the data?

Yes, but this does not apply to memory sticks. There are still devices that store data magnetically, such as traditional HDDs or the magnetic strips on payment cards. In their case, contact with a strong field can cause data loss. It is also worth mentioning that very strong industrial magnets can physically damage electronics, causing displacement of small components or short circuits, but these are extreme situations, far removed from everyday use.

Transfer Multisort Elektronik (TME) is one of the world’s largest global distributors of electronic components, electrotechnical parts, workshop equipment, and industrial automation. The catalog includes over 1,500,000 products from 1,300 leading manufacturers. TME’s modern logistics centers in Łódź and Rzgów (Poland), with a combined area of over 40,000 m², ship nearly 6,000 packages daily to customers in more than 150 countries.

TME also invests in the development of knowledge and skills of young engineers and electronics enthusiasts through the TME Education project, and supports the tech community by organizing the TechMasterEvent series, promoting innovation and experience exchange.

READ ALSO