+1 500 000 products in offer
7000 packages per day
+300 000 clients from 150 countries
It is worth replacing the flash drive when it starts to show signs of unstable operation, its speed deviates significantly from its original parameters, there are problems with writing data or the operating system suggests that formatting is necessary. Also when memory errors are detected or confidence in the media is lost, as continued use may lead to irreversible data loss.
Every memory stick has a limited technological life due to the nature of NAND flash memory. The most important limitation is programming and erasing cycles (P/E cycles). For typical media with MLC or TLC cells, this value ranges from a few thousand to tens of thousands of cycles. Once these are exceeded, data may be written erroneously and the media controller may start to mark more and more sectors as unusable. Symptoms of wear and tear are problems copying files, extended write times or sudden interruptions of operations , sometimes ending with an I/O error message. A common symptom is also that data has seemingly been saved, but when the flash drive is reconnected, the files disappear or have zero size. In some cases, the operating system reports that the flash drive needs to be formatted even when it was working correctly before. This could indicate a corrupted file system structure or a problem with the flash memory. If this situation occurs repeatedly, the media is no longer reliable.
Replacement of the flash drive is also advisable when its capacity and speed no longer meet the current needs of the user. Older models, operating in the USB 2.0 standard, offer very low read and write speeds compared to newer USB 3.2 Gen 1 or Gen 2 designs. This difference can be felt especially when transferring large multimedia files, ISO images or databases. Another case where replacement may be warranted is wear and tear mechanical, e.g. a loose USB connector, cracked Enclosures or scratches that can cause poor contacts and unstable operation. Such a flash drive can damage a computer's USB port or lead to accidental disconnection during data transfer. There is also the issue of data security. If the flash drive has been used for many years, in different computers and environments, there is a risk that it could have been infected with malware or has hidden system partitions. Even after formatting, some of these risks may remain, especially on older models with simple firmware. Any instance where a flash drive raises suspicions about its stability or data integrity should be a signal to replace it. The cost of buying a new, faster and more secure media is negligible compared to the potential loss of important data.
Transfer Multisort Elektronik (TME) is one of the world’s largest global distributors of electronic components, electrotechnical parts, workshop equipment, and industrial automation. The catalog includes over 1,500,000 products from 1,300 leading manufacturers. TME’s modern logistics centers in Łódź and Rzgów (Poland), with a combined area of over 40,000 m², ship nearly 6,000 packages daily to customers in more than 150 countries.
TME also invests in the development of knowledge and skills of young engineers and electronics enthusiasts through the TME Education project, and supports the tech community by organizing the TechMasterEvent series, promoting innovation and experience exchange.