+1 500 000 products in offer
6000 packages per day
+300 000 clients from 150 countries
Pulse (impulse) is a short signal of defined duration, characterized by a sudden rise and fall in the value of a physical quantity such as voltage, current, pressure, or light intensity. In electronics and signal theory, a pulse refers to an abrupt change in a signal over time, typically in the form of a single spike or a brief sequence, used to transmit information, trigger events, or synchronize processes in both digital and analog circuits.
Key pulse parameters—such as duration, amplitude, rise and fall time, and repetition frequency—determine its functional properties and influence on the system. In digital systems, pulses are fundamental elements representing logic states and are used for data transmission, clock timing, and control signal generation. In analog systems, a pulse can initiate dynamic responses in circuits, such as oscillations, filter reactions, or triggering of measurement functions.
Mathematically, a pulse is often modeled using the Dirac delta function, which idealizes an infinitely short and strong unit signal. However, in practical technical systems, a pulse has a finite duration and a specific shape determined by the characteristics of the source and the transmission medium. In measurement systems, pulses enable time-domain response analysis, dynamic system evaluation, and detection of extremely short-duration events.
Pulses have broad applications in telecommunications, electronics, automation, medicine, radar , and imaging technologies, where precise pulse generation and processing enable the development of advanced diagnostic, measurement, and control systems. In modern technologies, pulses are also the foundation of switching circuits, converters, digital systems, and devices requiring high temporal resolution.
Transfer Multisort Elektronik (TME) is one of the world’s largest global distributors of electronic components, electrotechnical parts, workshop equipment, and industrial automation. The catalog includes over 1,500,000 products from 1,300 leading manufacturers. TME’s modern logistics centers in Łódź and Rzgów (Poland), with a combined area of over 40,000 m², ship nearly 6,000 packages daily to customers in more than 150 countries.
TME also invests in the development of knowledge and skills of young engineers and electronics enthusiasts through the TME Education project, and supports the tech community by organizing the TechMasterEvent series, promoting innovation and experience exchange.