+1 500 000 products in offer

7000 packages per day

+300 000 clients from 150 countries

Quick Buy Favourites
Cart

Arithmetic logic unit (ALU) - definition

Arithmetic logic unit (ALU) is a fundamental component of a processor responsible for performing mathematical and logical operations on binary data. Within the central processing unit (CPU), the ALU serves as the execution unit, processing data according to instructions provided by the control unit. It performs operations such as addition, subtraction, bit shifting, comparisons, and logical functions including AND, OR, XOR, and NOT. All these operations occur at the binary level, enabling efficient data processing in digital systems.

The architecture of the ALU comprises a series of logic blocks and auxiliary registers that allow simultaneous processing of input signals, transfer of results to the destination registers, and generation of auxiliary signals such as carry, zero, overflow, and sign flags. These signals are used by other parts of the processor to make decisions regarding program flow or data handling.

The ALU operates in close cooperation with other processor units, such as general-purpose registers, the instruction decoder, and the memory management unit. Its performance and structure directly impact processing speed and the computational capabilities of the entire system. Depending on the architecture, the ALU can be designed as a single- or multi-function unit, operating sequentially or in parallel, and in advanced systems, multiple ALUs may be integrated to form multi-ALU configurations.

In modern processors, the ALU is part of larger computational structures such as vector units, pipelined units, or floating-point units, which expand its capabilities to support more complex mathematical operations. Despite technological advances and growing architectural complexity, the ALU remains an indispensable element of any digital system, executing core arithmetic and logic functions that are foundational to the operation of contemporary computing systems.

Transfer Multisort Elektronik (TME) is one of the world’s largest global distributors of electronic components, electrotechnical parts, workshop equipment, and industrial automation. The catalog includes over 1,500,000 products from 1,300 leading manufacturers. TME’s modern logistics centers in Łódź and Rzgów (Poland), with a combined area of over 40,000 m², ship nearly 6,000 packages daily to customers in more than 150 countries.

TME also invests in the development of knowledge and skills of young engineers and electronics enthusiasts through the TME Education project, and supports the tech community by organizing the TechMasterEvent series, promoting innovation and experience exchange.

READ ALSO