+1 500 000 products in offer

7000 packages per day

+300 000 clients from 150 countries

Quick Buy Favourites
Cart

Flip-flop (trigger circuit) - definition

Flip-flop (trigger circuit) is a fundamental component of digital logic electronics used to store a single bit of information in the form of two stable logic states. It operates as a bistable circuit, meaning it can remain in one of two possible states—representing a logical "0" or "1"—until a control signal forces a change. Flip-flops form the foundation of memory and sequential logic circuits, enabling the registration, synchronization, and time-based processing of binary data.

The operation of a flip-flop is based on a logic circuit composed of gates that use feedback to maintain their state. Unlike combinational logic gates, a flip-flop responds not only to current input values but also to the history of input changes, giving it memory-like behavior. A common classification distinguishes between asynchronous flip-flops (set independently of a clock signal) and synchronous flip-flops, which change state only at specific clock cycles—making them suitable for clocked digital systems.

The most commonly used types of flip-flops include SR, D, JK, and T, which differ in input configurations and response to control signals. They are used in registers, counters, finite state machines (FSMs), temporary memory units, and in all circuits requiring controlled storage or transition of logic states. Modern digital systems implement flip-flops as integrated circuits or as components defined in hardware description languages (HDLs), embedded within programmable logic devices.

Due to the importance of timing in digital systems, the design and placement of flip-flops must consider timing parameters such as propagation delay, setup time, hold time, and the risk of metastability. In digital architectures, a large number of flip-flops operating under a shared clock enable orderly and predictable data processing.

Transfer Multisort Elektronik (TME) is one of the world’s largest global distributors of electronic components, electrotechnical parts, workshop equipment, and industrial automation. The catalog includes over 1,500,000 products from 1,300 leading manufacturers. TME’s modern logistics centers in Łódź and Rzgów (Poland), with a combined area of over 40,000 m², ship nearly 6,000 packages daily to customers in more than 150 countries.

TME also invests in the development of knowledge and skills of young engineers and electronics enthusiasts through the TME Education project, and supports the tech community by organizing the TechMasterEvent series, promoting innovation and experience exchange.

READ ALSO