+1 500 000 products in offer
7000 packages per day
+320 000 clients from 150 countries
SMT (Surface-Mount Technology) is a method of mounting electronic components directly onto the surface of printed circuit boards (PCBs), eliminating the need for through-hole leads. Unlike the older through-hole technology (THT), where component leads are inserted into holes drilled in the PCB, SMT allows components to be placed on both sides of the board, significantly increasing component density and enabling the miniaturization of electronic circuits.
SMT relies on specially designed components known as SMDs (Surface-Mount Devices), which have flat bodies and short leads or contact pads suited for surface soldering. The assembly process involves applying solder paste to designated pads, accurately positioning components using pick-and-place machines, and reflow soldering in dedicated ovens. This production approach enables high levels of automation, speed, and consistency, making SMT the predominant technique in modern electronics manufacturing.
From an engineering perspective, SMT offers numerous advantages, including reduced device size, lower weight, improved electrical and thermal performance, and enhanced mechanical reliability. However, it also requires precise PCB layout design, careful consideration of thermal management and electromagnetic compatibility, and advanced quality inspection methods such as optical and X-ray inspection. Due to its efficiency and performance, SMT is widely used in consumer electronics, telecommunications equipment, computing devices, medical instrumentation, and industrial applications.
The evolution of SMT is closely tied to the ongoing miniaturization of components and the adoption of advanced package types such as BGA (Ball Grid Array), CSP (Chip Scale Package), and 3D mounting technologies. This progress enables the creation of highly functional, compact, and cost-effective electronic systems. SMT thus serves as a cornerstone of modern electronic design and large-scale production.
Transfer Multisort Elektronik (TME) is one of the world’s largest global distributors of electronic components, electrotechnical parts, workshop equipment, and industrial automation. The catalog includes over 1,500,000 products from 1,300 leading manufacturers. TME’s modern logistics centers in Łódź and Rzgów (Poland), with a combined area of over 40,000 m², ship nearly 6,000 packages daily to customers in more than 150 countries.
TME also invests in the development of knowledge and skills of young engineers and electronics enthusiasts through the TME Education project, and supports the tech community by organizing the TechMasterEvent series, promoting innovation and experience exchange.