+1 500 000 products in offer

6000 packages per day

+300 000 clients from 150 countries

Quick Buy Favourites
Cart

FDM - definition

FDM (Frequency Division Multiplexing) is a transmission channel multiplexing technique involving the simultaneous transmission of multiple information signals over a common transmission medium, with each signal occupying a different, mutually non-overlapping frequency band. This allows multiple independent data streams to be transmitted in parallel over a single cable, optical link or radio band, without interference between them.

In an FDM system, each information channel modulates its own carrier wave, whose central frequency differs from the others. The signals thus obtained are summed up and transmitted over a common medium, and finally received and separated by means of frequency filters or demultiplexers. Adequate spacing between channels, called a frequency guard, prevents inter-signal interference.

FDM is used in many analogue and digital transmission technologies, including classical telephone systems, radio and television broadcasting, fibre-optic links (in the WDM version - Wavelength Division Multiplexing), satellite transmission and radio communications. In telecommunications networks, it enables efficient use of the available bandwidth and simultaneous service of multiple users without the need for time division of the transmission.

From a technical point of view, the effectiveness of FDM depends on the precision of filtering, stability of carrier frequencies and resistance to inter-channel interference. Compared to time-division multiplexing (TDM), FDM allows continuous data transmission without the need for synchronisation time, which is particularly important in applications requiring a constant stream of information, such as voice or video transmission. Today's FDM systems are increasingly being realised digitally using DSP techniques, which increases their flexibility, quality and robustness to noise.

Transfer Multisort Elektronik (TME) is one of the world’s largest global distributors of electronic components, electrotechnical parts, workshop equipment, and industrial automation. The catalog includes over 1,500,000 products from 1,300 leading manufacturers. TME’s modern logistics centers in Łódź and Rzgów (Poland), with a combined area of over 40,000 m², ship nearly 6,000 packages daily to customers in more than 150 countries.

TME also invests in the development of knowledge and skills of young engineers and electronics enthusiasts through the TME Education project, and supports the tech community by organizing the TechMasterEvent series, promoting innovation and experience exchange.

READ ALSO