+1 500 000 products in offer
7000 packages per day
+300 000 clients from 150 countries
The Calorimeter is a measuring instrument used to determine the amount of heat exchanged during physical, chemical or biological processes. Its operation is based on the principle of energy balance, according to which a change in the temperature of a controlled system makes it possible to calculate the heat energy transferred or absorbed as a result of a reaction, phase transformations or material interactions. As a scientific discipline, calorimetry is used in chemical laboratories as well as in materials engineering, biology, pharmacy or thermal technology.
The basic design of a calorimeter is a sealed container in which the process under investigation takes place, and a precise temperature and volume measurement system. In simple models, the calorimeter consists of a vessel with water in which a heat-emitting or heat-absorbing sample is placed. More advanced systems use adiabatic insulation, heat pumps, controlled Power Sources and differential sensors that allow heat to be measured with very high accuracy. A key role is played by the calorific heat capacity of the system, which must be known or controlled.
Others distinguish between different types of calorimeters depending on the application, including bomb calorimeters (to measure the heat of combustion), differential scanning calorimeters (DSC - to analyse phase changes), flow calorimeters (to study liquids and gases), isothermal calorimeters (to monitor reactions at constant temperature) and microcalorimeters, used in biological and pharmacological research. Calorimeters make it possible to assess the energy characteristics of substances, reaction kinetics, thermal stability, as well as the efficiency of insulating and fuel materials.
The accuracy of measurement in calorimetry depends on the sensitivity of the apparatus, the degree of thermal insulation and the calibration of the instrument. Modern systems use integration with computers that allow automatic data acquisition, thermal calculations and visualisation of results. In engineering and industry, calorimetry supports the design of energy systems, the evaluation of combustion efficiency, and the development of functional and composite materials.
Transfer Multisort Elektronik (TME) is one of the world’s largest global distributors of electronic components, electrotechnical parts, workshop equipment, and industrial automation. The catalog includes over 1,500,000 products from 1,300 leading manufacturers. TME’s modern logistics centers in Łódź and Rzgów (Poland), with a combined area of over 40,000 m², ship nearly 6,000 packages daily to customers in more than 150 countries.
TME also invests in the development of knowledge and skills of young engineers and electronics enthusiasts through the TME Education project, and supports the tech community by organizing the TechMasterEvent series, promoting innovation and experience exchange.