+1 500 000 products in offer

7000 packages per day

+300 000 clients from 150 countries

Quick Buy Favourites
Cart

Comparators - definition

A Comparator is an Instrumentation whose function is to compare two input voltages and generate a logic signal at the output corresponding to the result of the comparison. It works by detecting the difference between the voltages given to the non-inverting and inverting input, returning a high signal ('1' logic state) or a low signal ('0') depending on which voltage is greater. A comparator belongs to the group of non-linear circuits and often has a structure similar to an Operational amplifier, but with different operating characteristics - its output is not linearly dependent on the voltage difference, but takes on the marginal values in a switching manner.

In practical applications, comparators act as threshold detectors, analogue-to-digital converters, pulse generators and analogue logic elements. Their fast operation enables them to be used in clocking, monitoring, measuring and Automation systems, where fast response to exceeding a set voltage value is important. Comparators with hysteresis, which counteract switching oscillations in the event of interference or noise in the input signal, are also used in advanced designs.

Unlike a classical operational amplifier, a comparator is not designed to operate in linear mode but in the saturation zone, allowing it to act as a switching circuit. Its output is often of the open collector or drain type, allowing it to be easily adjusted to different logic levels by selecting a pull-up resistor. In digital systems, comparators are used to convert analogue signals to digital logic levels and to generate synchronising signals.

Due to their simplicity of design and speed of operation, comparators are commonly integrated into integrated circuits, both as stand-alone components and as components of larger analogue-to-digital structures such as ADCs, voltage regulators, sensors and measurement systems. The selection of parameters such as rise time, offset voltage and bandwidth is crucial for their correct operation in a specific application.

Transfer Multisort Elektronik (TME) is one of the world’s largest global distributors of electronic components, electrotechnical parts, workshop equipment, and industrial automation. The catalog includes over 1,500,000 products from 1,300 leading manufacturers. TME’s modern logistics centers in Łódź and Rzgów (Poland), with a combined area of over 40,000 m², ship nearly 6,000 packages daily to customers in more than 150 countries.

TME also invests in the development of knowledge and skills of young engineers and electronics enthusiasts through the TME Education project, and supports the tech community by organizing the TechMasterEvent series, promoting innovation and experience exchange.

READ ALSO