+1 500 000 products in offer
7000 packages per day
+300 000 clients from 150 countries
The PID (Proportional-Integral-Derivative) regulator is a control algorithm used in Automation and systems engineering to precisely regulate process variables by minimising the error between the setpoint and the current measured value. Its operation is based on three components: proportional (P), integral (I) and differential (D), which work together to dynamically adjust the control signal so that the system achieves stability, fast responses and minimal overshoot.
The proportional member produces a control signal proportional to the error value, which provides a direct response to deviations from the setpoint. The integrating member adds up the error over time, eliminating static deviation and enabling accurate setpoint tracking to be achieved. The differentiating member, on the other hand, predicts future changes in the error, acting as a mechanism to dampen oscillations and increase system stability.
By appropriately tuning the gain parameters of the individual members, the PID regulator can be adapted to a wide range of dynamic systems, including thermal, hydraulic, electrical and mechanical processes. In engineering practice, PID is an essential tool used in temperature, pressure, speed, position control systems and industrial applications such as robotics, actuator control and manufacturing processes.
In modern control systems, the PID controller can be implemented both in hardware (PLC Drivers modules, dedicated systems) and software form (algorithms in SCADA systems, embedded systems and microprocessor controllers), often with additional adaptive or automatic real-time parameter tuning functions.
Transfer Multisort Elektronik (TME) is one of the world’s largest global distributors of electronic components, electrotechnical parts, workshop equipment, and industrial automation. The catalog includes over 1,500,000 products from 1,300 leading manufacturers. TME’s modern logistics centers in Łódź and Rzgów (Poland), with a combined area of over 40,000 m², ship nearly 6,000 packages daily to customers in more than 150 countries.
TME also invests in the development of knowledge and skills of young engineers and electronics enthusiasts through the TME Education project, and supports the tech community by organizing the TechMasterEvent series, promoting innovation and experience exchange.