+1 500 000 products in offer
6000 packages per day
+300 000 clients from 150 countries
Thermodynamics is the branch of physics concerned with the study of energy, its transformations and the interplay between heat, work and the properties of matter in macroscopic systems. Its primary objects of analysis are thermodynamic equilibrium states and the processes that lead to changes in these states as a result of the exchange of energy and matter with the environment. Thermodynamics provides fundamental laws and mathematical models that describe how energy flows and how it affects the properties of matter, without reference to the detailed molecular structure of the systems under study.
The description of thermodynamic systems is based on concepts of macroscopic quantities such as pressure, volume, temperature, internal energy, entropy and enthalpy, which are related to each other through equations of state and conservation principles. Classical thermodynamics, also known as macroscopic thermodynamics, uses these parameters to analyse processes such as phase transformations, chemical reactions, gas expansion or heat flow.
Central to thermodynamics are its four fundamental principles, known as the principles of thermodynamics. The zero principle defines the concept of temperature and the condition of thermal equilibrium. The first principle expresses the principle of conservation of energy, stating that the change in internal energy of a system is equal to the difference between the heat supplied to it and the work done by the system. The second principle defines the direction of natural processes, introducing the concept of entropy and indicating that spontaneous processes occur in the direction of increasing entropy. The third principle, concerning the conservation of entropy at a temperature of absolute zero, formulates the constraints on reaching this state.
In engineering and technology, thermodynamics is central to the design and analysis of thermal machines such as internal combustion engines, steam turbines, refrigerators, heat pumps and power systems, where optimising energy efficiency and minimising losses are overriding design goals. In physical chemistry, chemical thermodynamics studies the energy changes that accompany chemical reactions, allowing the prediction of reaction direction and the calculation of parameters such as reaction enthalpy, Gibbs free energy and chemical equilibrium.
Statistical thermodynamics, an extension of the classical approach, introduces microscopic analysis by applying the methods of mathematical statistics to ensembles of large numbers of molecules, making it possible to derive macroscopic properties of systems from equations describing microscopic energy states. This field explains the fundamental origin of entropy as a measure of the number of available microscopic states of a system and enables the description of phenomena in quantum, critical and far-from-equilibrium systems.
In modern research, thermodynamics finds application in the analysis of nanoscale processes, the dynamics of biological systems, information theory and materials technology, where an understanding of the transport of energy and matter at a fundamental level is crucial to the design of new devices and systems with high energy efficiency. The extension of thermodynamic principles to non-linear and dynamic systems enables the modelling of real processes in complex natural and technological systems.
Transfer Multisort Elektronik (TME) is one of the world’s largest global distributors of electronic components, electrotechnical parts, workshop equipment, and industrial automation. The catalog includes over 1,500,000 products from 1,300 leading manufacturers. TME’s modern logistics centers in Łódź and Rzgów (Poland), with a combined area of over 40,000 m², ship nearly 6,000 packages daily to customers in more than 150 countries.
TME also invests in the development of knowledge and skills of young engineers and electronics enthusiasts through the TME Education project, and supports the tech community by organizing the TechMasterEvent series, promoting innovation and experience exchange.