+1 500 000 products in offer

7000 packages per day

+300 000 clients from 150 countries

Quick Buy Favourites
Cart

Thermometer - definition

Thermometer is a measuring instrument for determining the temperature of a body, substance or environment, based on physical phenomena in which a change in temperature produces a measurable change in another quantity such as volume, resistance, pressure, radiation or thermoelectric voltage. It is one of the basic Measuring Tools in life sciences, engineering, medicine and everyday life.

The construction and principle of operation of a thermometer depend on the temperature sensing mechanism used. Classical liquid thermometers take advantage of the expansion of the liquid (e.g. mercury or alcohol) in the capillary, while electronic systems rely on resistance sensors (RTDs), thermistors or thermocouples for measurement. Each of these methods converts a temperature change into an electrical, mechanical or optical signal that can be further processed, recorded or displayed.

Others thermometers can be calibrated in different units, most commonly degrees Celsius, Fahrenheit or kelvin (K), depending on the application and standards. High measurement accuracy and repeatability require consideration of non-linear phenomena, the influence of ambient conditions, and adequate compensation for the influence of other variables, e.g. humidity or pressure.

In modern systems, thermometers are often part of larger measurement and control systems, where they interact with microprocessors, A/D converters and communication interfaces. Depending on the design, they can enable local or remote measurement, operate in a contact or non-contact manner (e.g. infrared thermometers at ) and handle dynamic temperature changes in real time.

The applications of thermometers range from industrial process control, scientific research and environmental monitoring to domestic and clinical applications, making them an indispensable part of modern measurement technology.

Transfer Multisort Elektronik (TME) is one of the world’s largest global distributors of electronic components, electrotechnical parts, workshop equipment, and industrial automation. The catalog includes over 1,500,000 products from 1,300 leading manufacturers. TME’s modern logistics centers in Łódź and Rzgów (Poland), with a combined area of over 40,000 m², ship nearly 6,000 packages daily to customers in more than 150 countries.

TME also invests in the development of knowledge and skills of young engineers and electronics enthusiasts through the TME Education project, and supports the tech community by organizing the TechMasterEvent series, promoting innovation and experience exchange.

READ ALSO