+1 500 000 products in offer

7000 packages per day

+300 000 clients from 150 countries

Quick Buy Favourites
Cart

Kelvin (K) - definition

Kelvin (K) is the SI base unit of thermodynamic temperature, defined based on the Boltzmann constant—a fundamental physical constant that relates temperature to the energy of particles. One kelvin corresponds to the same temperature change as one degree Celsius; however, the kelvin scale starts at absolute zero, which represents the complete absence of molecular kinetic energy. Zero kelvin is the lowest possible temperature, at which all thermal motion in matter theoretically ceases, although it has never been reached in practice.

The kelvin is an absolute unit, independent of reference points based on the properties of water, as is the case with the Celsius or Fahrenheit scales. It is named after Lord Kelvin (William Thomson), who in the 19th century proposed an absolute temperature scale as a consequence of thermodynamic. principles. In its modern form, since 2019, the kelvin has been defined by assigning a fixed numerical value to the Boltzmann constant, ensuring greater precision and consistency in physical science measurements.

In technical and engineering applications, the kelvin is used to describe absolute temperature in thermal processes, analyze material properties, characterize states of matter, and in statistical mechanics. The kelvin scale is widely used in science and engineering, particularly where it is essential to distinguish absolute temperature from relative temperature. This unit is mandatory in many fields of metrology, nuclear physics, cryogenics, astrophysics, and materials engineering, where accurate temperature determination impacts quality, safety, and process predictability.

Transfer Multisort Elektronik (TME) is one of the world’s largest global distributors of electronic components, electrotechnical parts, workshop equipment, and industrial automation. The catalog includes over 1,500,000 products from 1,300 leading manufacturers. TME’s modern logistics centers in Łódź and Rzgów (Poland), with a combined area of over 40,000 m², ship nearly 6,000 packages daily to customers in more than 150 countries.

TME also invests in the development of knowledge and skills of young engineers and electronics enthusiasts through the TME Education project, and supports the tech community by organizing the TechMasterEvent series, promoting innovation and experience exchange.

READ ALSO