+1 500 000 products in offer
7000 packages per day
+300 000 clients from 150 countries
Kinetic energy is a form of mechanical energy associated with the motion of a body relative to a given frame of reference. It quantifies the ability of a moving object to perform work as a result of its motion and depends on both its mass and velocity. In classical mechanics, the kinetic energy of an object with constant mass increases proportionally to the square of its velocity, meaning that even a small increase in speed results in a significant rise in energy.
From a physical standpoint, kinetic energy reflects the effect of forces acting on a body during its displacement and is one of the fundamental quantities describing the dynamics of systems. In closed systems, where no external forces act or their net effect is zero, total kinetic energy can be transformed into other forms of energy—such as potential or internal energy—without violating energy conservation. Changes in kinetic energy are directly related to acceleration, deceleration, and interactions such as collisions or force exchanges between bodies.
In engineering, kinetic energy plays a crucial role in the design of mechanical systems, the calculation of dynamic parameters of machines, crash safety analysis, fluid mechanics, and aerospace engineering. It is also relevant in electrical engineering, particularly in evaluating the performance of rotating machinery such as motors and generators. On a microscopic scale, in statistical physics and thermodynamics, the kinetic energy of particles is closely linked to temperature and the energy state of matter.
Transfer Multisort Elektronik (TME) is one of the world’s largest global distributors of electronic components, electrotechnical parts, workshop equipment, and industrial automation. The catalog includes over 1,500,000 products from 1,300 leading manufacturers. TME’s modern logistics centers in Łódź and Rzgów (Poland), with a combined area of over 40,000 m², ship nearly 6,000 packages daily to customers in more than 150 countries.
TME also invests in the development of knowledge and skills of young engineers and electronics enthusiasts through the TME Education project, and supports the tech community by organizing the TechMasterEvent series, promoting innovation and experience exchange.