+1 500 000 products in offer

7000 packages per day

+300 000 clients from 150 countries

Quick Buy Favourites
Cart

Microchip Technology at TME – security systems

Date of publication: 06-11-2026 🕒 7 min read

In terms of meeting cybersecurity requirements Microchip Technology offers its customers secure hardware solutions, software tools, services helping designers implement trusted device identity, Secure Boot, authentication, protection of credentials stored in the device, secure provisioning and other fundamental security functions.

Microchip Technology offering

Cyber Resilience Act

Currently, the requirement to ensure cybersecurity for embedded devices in European Union countries is no longer merely a matter of good practice, but is also becoming a legal obligation. At the end of 2024, the EU CRA regulation (Cyber Resilience Act) came into force, establishing mandatory cybersecurity requirements for products with digital elements placed on the EU market. The regulation covers both hardware and software, as well as related remote data processing solutions. It places a large part of the responsibility for device security on its manufacturer and aims to ensure that cybersecurity is considered already at the device design stage and subsequently maintained throughout its entire period of use. The manufacturer is required to conduct a cybersecurity risk assessment, design the product in accordance with the principles of “secure by design” and “secure by default”, reduce the potential attack surface, protect data and implement authentication mechanisms, as well as ensure an effective vulnerability management process throughout the declared support (lifetime) period of the product. The product should be placed on the market without known vulnerabilities that could be exploited by unauthorized parties, and the manufacturer must ensure appropriate procedures for identifying and eliminating threats during the support period. For example, a simple temperature controller, an industrial Ethernet controller, an IP camera or a network gateway will require entirely different levels of protection. At the same time, the manufacturer should have procedures enabling the identification of potential vulnerabilities, their analysis, and the remediation of detected vulnerabilities by providing users with appropriate patches and updates.

From a practical point of view, for a device designer this means that it should have the following mechanisms:

  1. Root of Trust: the device should have a reliable starting point for the security process, preferably hardware-based. This may be a protected MCU area, a security chip (secure element) or a dedicated security module.
  2. Secure Boot: the processor should launch only firmware whose authenticity and integrity have been cryptographically verified.
  3. Signed firmware updates: having a bootloader alone is not enough. Updated firmware should be digitally signed, and the device should reject unauthorized images.
  4. Secure key storage: private keys, symmetric keys and other confidential cryptographic data should not be stored in unprotected Flash memory areas.
  5. Debug interface control: JTAG, SWD, UART or the bootloader should be disabled or appropriately secured in a production device.
  6. Communication protection: communication with the cloud, a mobile application or other devices should use modern cryptography, such as TLS, DTLS or appropriate application-layer protocols.
  7. Device authentication: a unique identity for each device is increasingly used – a key or certificate assigned already during production.
  8. Principle of Least Privilege: individual software blocks should have only the permissions that are actually needed.
  9. Attack surface minimization: unnecessary ports, protocols, services and interfaces should be disabled.
  10. Update mechanism throughout the product support period: the manufacturer must assume that vulnerabilities will be discovered after the product has already been sold.

Microchip Technology's approach to cybersecurity is based on building a chain of trust, founded on Root of Trust – a trusted hardware or software element enabling verification of the integrity and authenticity of subsequent system components. The manufacturer's approach can be simplified into the following chain:

Hardware Root of Trust → Secure Boot → Key protection → Device authentication → Secure communication → Secure firmware update → Product lifecycle management

Diagram showing the use of Trust Manager and keySTREAM throughout the product lifecycle: from concept and development, through production and use, to support and decommissioning. Source: Microchip Technology

In the hardware area, Microchip Technology offers solutions with varying levels of sophistication: from security features built into PIC and AVR microcontrollers, through microcontrollers with dedicated security subsystems, to external Secure Element chips, HSMs and dedicated Platform Root of Trust controllers.

Multi-layered approach to security

Microchip Technology solutions can be arranged into several groups:

Solution group Examples Main function in the security system
MCUs with basic security features PIC, AVR, e.g. AVR DU code protection, programming and debugging lockout (PDID), secure update
MCUs with advanced security mechanisms SAM L11, PIC32CM LS secure boot, TrustZone, code and data isolation, hardware cryptography
MCUs with HSM / secure subsystem PIC32CZ CA90 hardware-isolated cryptographic operations and key storage
SecureElement / CryptoAuthentification ATECC608, TA101, ECC204, SHA10x key storage, authentication, hardware trust anchor
Platform Root of Trust CEC173x, TS1800, TS50x platform verification, secure boot, attestation, firmware protection
Secure provisioning Trust&GO, TrustFLEX, TrustCUSTOM, TrustMANAGER secure assignment and management of keys and device identities

32-bit PIC32 family microcontrollers

Microcontrollers from the PIC32 family offer diverse security mechanisms, from basic protection of memory and program code to advanced cryptographic functions, secure boot (Secure Boot) and isolation of system resources. Depending on the series, they can be used in applications requiring software, data and communication protection, including IoT devices and industrial systems.

PIC32TME family

Table comparing the security features of PIC and AVR microcontrollers as well as ECC608 and TA010 chips. Source: Microchip Technology

Microchip Technology microprocessors

Microchip Technology microprocessors designed for more advanced embedded systems are equipped with mechanisms supporting software and data protection. These include secure boot, hardware acceleration of cryptographic operations, and solutions enabling the isolation of selected system resources. These features are particularly important in devices operating under operating systems that require reliable communication and protection against unauthorized access.

Microprocessor offering at TME

Overview of Microchip security solutions for FPGA devices, microcontrollers and microprocessors, TPM modules and cryptography. Source: Microchip Technology

Microchip Technology digital signal microcontrollers

dsPIC digital signal microcontrollers combine real-time control functions with software and data protection mechanisms. Depending on the family, they offer, among other things, memory protection, secure boot, protection against unauthorized debugging and hardware support for cryptographic operations. These solutions are used primarily in motor control systems, power electronics and industrial automation.

dsPIC microcontrollers

Comparison of the security features of digital signal controllers from the dsPIC33 families. Source: Microchip Technology

Microchip Technology security chips (secure key storage/authentication)

Dedicated Microchip Technology security chips complement the mechanisms integrated into microcontrollers and microprocessors. These solutions enable, among other things, secure storage of cryptographic keys, device authentication and verification of software integrity. By separating selected security functions into dedicated chips, it is possible to reduce the risk of confidential data exposure even if the security of the main processor is compromised.

Authentication chips

Microchip security chip portfolio including Secure Elements, Platform Root of Trust and embedded controllers supporting key management and TrustZone. Source: Microchip Technology

One of Microchip Technology's most important groups of security products is the CryptoAuthentication family of chips.

Their primary task is to store the most sensitive cryptographic data in an area isolated from the application firmware. For example, a private key can be generated or stored inside a Secure Element and never needs to leave the chip. Instead of reading the key, the processor can only request an operation:

Data → Secure Element → cryptographic operation → result

As a result, taking control of the microcontroller firmware does not necessarily automatically mean taking control of the device's private key.

ATECC608

ATECC608 is one of the most widely used Secure Element chips in the Microchip Technology portfolio.

The chip can be connected to virtually any MCU or MPU via I²C or a single-wire interface. A typical architecture may therefore be:

MCU → ATECC608 → network / cloud

ATECC608 stores the device's cryptographic identity, while the microcontroller is responsible for the actual application.

Transfer Multisort Elektronik (TME) is one of the world’s largest global distributors of electronic components, electrotechnical parts, workshop equipment, and industrial automation. The catalog includes over 1,500,000 products from 1,300 leading manufacturers. TME’s modern logistics centers in Łódź and Rzgów (Poland), with a combined area of over 40,000 m², ship nearly 6,000 packages daily to customers in more than 150 countries.

TME also invests in the development of knowledge and skills of young engineers and electronics enthusiasts through the TME Education project, and supports the tech community by organizing the TechMasterEvent series, promoting innovation and experience exchange.

rightColumnPicture rightColumnPicture

READ ALSO