+1 500 000 products in offer

6000 packages per day

+300 000 clients from 150 countries

Quick Buy Favourites
Cart

Heat exchange - definition

Heat exchange is the physical process of transferring thermal energy between systems or elements at different temperatures. This phenomenon occurs spontaneously and always in the direction from a higher-temperature body to a lower-temperature body, until a state of thermal equilibrium is reached. Heat transfer plays a fundamental role in thermal engineering, power generation, refrigeration, air conditioning, industrial processes and electronic systems requiring the dissipation of excess heat.

According to physical mechanisms, heat transfer can take place in three basic ways: by conduction, convection and radiation. Conduction (conduction) involves the direct transfer of energy within a solid body or between contacting bodies, resulting from temperature differences and micro vibrations of molecules. Convection refers to the transfer of heat in liquids and gases, where energy is transferred by the mass movement of the medium - natural or forced. Radiation is the emission of energy in the form of electromagnetic waves, which does not require the presence of a material medium and can occur in a vacuum.

Heat transfer is described quantitatively using concepts such as heat flux, conduction coefficient, heat transfer coefficient and dimensionless numbers, e.g. Nusselt, Prandtl or Reynolds numbers, used in heat flow analysis. This issue is analysed in the context of Fourier's law (for conduction), Newton's law (for convection) and Stefan-Boltzmann's law (for radiation).

In the design of technical equipment, consideration of heat transfer allows for efficient energy management, prevention of overheating of components, optimisation of process efficiency and improved operational safety. The selection of appropriate materials, geometries and flow parameters is a key element of engineering thermal calculations and heat transfer system design.

Heat Exchangers

Transfer Multisort Elektronik (TME) is one of the world’s largest global distributors of electronic components, electrotechnical parts, workshop equipment, and industrial automation. The catalog includes over 1,500,000 products from 1,300 leading manufacturers. TME’s modern logistics centers in Łódź and Rzgów (Poland), with a combined area of over 40,000 m², ship nearly 6,000 packages daily to customers in more than 150 countries.

TME also invests in the development of knowledge and skills of young engineers and electronics enthusiasts through the TME Education project, and supports the tech community by organizing the TechMasterEvent series, promoting innovation and experience exchange.

READ ALSO