+1 500 000 products in offer

7000 packages per day

+320 000 clients from 150 countries

Quick Buy Favourites
Cart

Connectors p-n - definition

Connectors p-n is a fundamental semiconductor structure, formed at the interface between two areas of the same semiconductor material with opposite types of conductivity: p-type (dominated by holes as majority carriers) and n-type (where majority carriers are electrons). This creates a potential barrier and a depleted layer, that is the area without free carriers, which acts as a barrier and determines the directionality of current conduction.

In thermodynamic equilibrium, with no external voltage applied, in the p-n junction an internal potential is established due to diffusion of carriers: electrons from the n region move to the p region, and holes vice versa, leading to recombination and the formation of an area without free charges. This region - called the barrier layer - contains the exposed dopant ions, forming an embedded electric field, which counteracts the further flow of carriers.

When the p connector is polarised-n junction in the conduction direction (positive potential to the p part), the potential barrier is lowered, allowing current to flow. When polarised in the negative direction, the barrier increases, and the current is limited to small leakage values. These properties make, that the p-n junction acts as a one-way valve and is the basis for the operation of many semiconductor components, such as rectifier diodes, lEDs, photodiodes, bipolar transistors (BJT) and Unipolar transistors (MOSFET), as well as radiation detectors or light sensors.

Connector parameters p-n - including barrier layer width, potential barrier height and current-voltage characteristics - depend-characteristics - depend on type and level of doping, temperature and geometry of the system. Understanding the behaviour of the p-n junction is crucial for the analysis and design of electronic circuits for both low- and high-power signals, and high power signals.

Transfer Multisort Elektronik (TME) is one of the world’s largest global distributors of electronic components, electrotechnical parts, workshop equipment, and industrial automation. The catalog includes over 1,500,000 products from 1,300 leading manufacturers. TME’s modern logistics centers in Łódź and Rzgów (Poland), with a combined area of over 40,000 m², ship nearly 6,000 packages daily to customers in more than 150 countries.

TME also invests in the development of knowledge and skills of young engineers and electronics enthusiasts through the TME Education project, and supports the tech community by organizing the TechMasterEvent series, promoting innovation and experience exchange.

READ ALSO