+1 500 000 products in offer
6000 packages per day
+300 000 clients from 150 countries
An Electric Field is a vector physical field that describes the electric interaction exerted by electric charges on other charges within its range. It is a form of matter existence that extends in space around a source of charge and manifests itself through a force acting on other electric charges. The magnitude of this force depends on the value of the charge experiencing the field and the intensity of the field at a given point.
Mathematically, the electric field is defined as the force acting on a unit positive charge placed at a given point in space. The electric field vector has a direction in line with the direction of this force and its value is given by the formula E = F/q, where E is the electric field strength, F is the force acting on the test charge q. The unit of field strength in SI is volts per metre (V/m).
Sources of electric field can be both static and dynamic charges, as well as alternating magnetic fields, according to the laws of electromagnetism described by Maxwell's equations. In the case of a field generated by a single point charge, its intensity decreases inversely proportional to the square of the distance from the source and is directed radially - outwards for a positive charge and inwards for a negative charge.
An electric field can exist both in a vacuum and in material media, where its interaction is modified by the dielectric properties of the material. In the presence of insulating materials, the field causes a polarisation phenomenon, affecting the distribution of internal charges and changing the effective electrical permeability of the environment. Electric field lines are a conventional graphical representation of the direction and intensity of the field - they do not intersect and always start from positive charges and end at negative charges.
The electric field plays a fundamental role in electrotechnics, electronics, electrostatics and solid state physics. In engineering, it is used in Capacitors, sensing systems, shielding, drive systems and in high voltage technology, where control of its distribution is crucial to the safety and efficiency of equipment.
Transfer Multisort Elektronik (TME) is one of the world’s largest global distributors of electronic components, electrotechnical parts, workshop equipment, and industrial automation. The catalog includes over 1,500,000 products from 1,300 leading manufacturers. TME’s modern logistics centers in Łódź and Rzgów (Poland), with a combined area of over 40,000 m², ship nearly 6,000 packages daily to customers in more than 150 countries.
TME also invests in the development of knowledge and skills of young engineers and electronics enthusiasts through the TME Education project, and supports the tech community by organizing the TechMasterEvent series, promoting innovation and experience exchange.