+1 500 000 products in offer

6000 packages per day

+300 000 clients from 150 countries

Quick Buy Favourites
Cart

Magnetic field - definition

A Magnetic Field is a vector physical field describing the force effects on moving electric charges and on bodies having a magnetic moment. It is generated by electric currents, alternating electric fields or natural sources of magnetism, such as permanent magnets. The magnetic field does not exist as an independent substance, but as a manifestation of the electromagnetic variation of space in which the Lorentz force acts on charged particles in motion.

The magnetic field vector determines both the direction and the value of the magnetic force acting on a unit charge moving at a unit speed, according to the right-hand rule. Mathematically it is defined by the formula F = q(v × B), where F is the magnetic force, q is the electric charge, v is the particle's velocity vector and B is the magnetic induction vector. The SI unit of magnetic field is tesla (T).

The magnetic field is an intrinsic component of the electromagnetic field and is closely related to the electric field, as described by Maxwell's equations. The magnetic field does not have a direct effect on charges at rest, but on moving charges and currents, which is the basis for the operation of electric motors, generators, transformers and many sensors.

Graphically, the magnetic field is represented by field force lines that form closed loops and never intersect. These lines extend from the north pole of the field source and return to the south pole, creating a spatial representation of the distribution of magnetic interaction. In the case of a current-carrying conductor, the field lines form circles around the conductor, according to the helical rule.

In the presence of ferromagnetic materials, the field can be enhanced by the phenomenon of magnetisation, leading to a concentration of field lines inside these materials. Magnetic field phenomena play a key role in solid state physics, electromagnetic engineering, communication technology, power systems and magnetic memory devices.

Transfer Multisort Elektronik (TME) is one of the world’s largest global distributors of electronic components, electrotechnical parts, workshop equipment, and industrial automation. The catalog includes over 1,500,000 products from 1,300 leading manufacturers. TME’s modern logistics centers in Łódź and Rzgów (Poland), with a combined area of over 40,000 m², ship nearly 6,000 packages daily to customers in more than 150 countries.

TME also invests in the development of knowledge and skills of young engineers and electronics enthusiasts through the TME Education project, and supports the tech community by organizing the TechMasterEvent series, promoting innovation and experience exchange.

READ ALSO