+1 500 000 products in offer
6000 packages per day
+300 000 clients from 150 countries
Conductor is a material or substance characterized by its ability to freely conduct electric charges due to the presence of charge carriers such as electrons or ions. In the case of metals, which are the most common conductors, electrical conductivity results from free electrons moving within the crystal lattice. Their motion under the influence of an applied electric field generates an electric current, and the resistance encountered during this movement depends on the material's physical and chemical properties.
The conductive properties of a material are defined by its electrical conductivity—the inverse of resistivity, which quantifies the resistance offered by a unit volume. The best conductors include copper and silver, widely used in power engineering, electronics, and telecommunications due to their low resistance and high durability. Specialized applications may also employ aluminum, gold, and, under specific conditions, graphene or superconductors.
Conductors may take the form of wires, printed circuit traces, connectors, electrodes, or composite materials used in complex electronic structures. Their properties affect not only current flow but also phenomena such as heating, power loss, electromagnetic shielding, and electromagnetic compatibility of systems. Besides ideal conductors, there are materials that exhibit conductive behavior only under certain conditions, such as semiconductors or electrolytes, whose performance depends on external factors like temperature, humidity, or electric field.
From the perspective of solid-state theory, conductivity in metals is explained using the band model, where the conduction band and valence band overlap or are separated by a very narrow energy gap, allowing electrons to easily transition to a conductive state. Understanding these properties enables the design of materials tailored to specific technical and industrial applications.
Transfer Multisort Elektronik (TME) is one of the world’s largest global distributors of electronic components, electrotechnical parts, workshop equipment, and industrial automation. The catalog includes over 1,500,000 products from 1,300 leading manufacturers. TME’s modern logistics centers in Łódź and Rzgów (Poland), with a combined area of over 40,000 m², ship nearly 6,000 packages daily to customers in more than 150 countries.
TME also invests in the development of knowledge and skills of young engineers and electronics enthusiasts through the TME Education project, and supports the tech community by organizing the TechMasterEvent series, promoting innovation and experience exchange.